Can we do DDR4 calibration IMX8MP custom board, without USB OTG?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we do DDR4 calibration IMX8MP custom board, without USB OTG?

Jump to solution
1,915 Views
abhiroopnray
Contributor III

We have made a custom board from IMX8MP. 

In the board there is no USB OTG available. 

USB hosts are available though.

Is there any way to do DDR calibration using MScale DDR  Tool, without USB OTG?

0 Kudos
1 Solution
1,869 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

No, it is not possible as specified in the DDR stress tool user guide:

It is a program running on the PC side which downloads a test image to the i.MX series processor’s internal RAM through a USB connection.

Best regards,
Aldo.

View solution in original post

4 Replies
1,833 Views
abhiroopnray
Contributor III

Hello @AldoG 

 

Thank you for the response.

I would like to know, if there is any way we can connect the board with Linux OS?
I can see MScale DDR  Tool is only available in .exe format. Is there any variant for Linux OS?

0 Kudos
1,811 Views
AldoG
NXP TechSupport
NXP TechSupport

Hi,

You may try using the config tool for i.MX, available for download here:
https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX

This tool support DDR stress test for i.MX8M family devices.

Best regards,
Aldo.

0 Kudos
1,870 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

No, it is not possible as specified in the DDR stress tool user guide:

It is a program running on the PC side which downloads a test image to the i.MX series processor’s internal RAM through a USB connection.

Best regards,
Aldo.

1,109 Views
siegfried_buerger
Contributor II
Does it also work with a simple USB device interface?
0 Kudos