The imx28evk comes with a 800x480 LCD, but I would like to drive a 800x600 SVGA display. I know the reference manual specifies 800x480 as the maximum, and I presume the limitation is the DOTCLK frequency, right?
Is this possible to do by e.g. by choosing a lower (perhaps non-standard) frame rate, thus lowering the DOTCLK frequency? Does anyone know what the maximum DOTCLK specification is for the imx287?
Hi Cheng,
i know that this is a quite old thread but your display-driver with DCP support sounds interesting to me.
I have a application with sound and display out/input and I recently ran into performance issues with the imx28.
I want to use the DCP to offload some operation from the cpu. First step would to use it in the framebuffer-driver of the imx28.
Can you provide me some information about your display-driver?
Thanks!
Christian
OK, thanks.
The default 800x480 setting has a dot clock of approx 1/30 nsec = 33.3 MHz.
Frame rate = 33.3 MHz / (800+10+164+89) / (480+10+10+23) = 59.9 Hz
If you increase the resolution to 800x600, while keeping the same dot clock, the frame rate will be:
Frame rate = 33.3 MHz / (800+10+164+89) / (600+10+10+23) = 48.7 Hz
Hi John,
I have a imx28evk board with a Seiko 4.3" lcd panel. I have a question about the dot clock frequency of lcd panel.
If I set for example DOTCLK_V_ACTIVE to 480,DOTCLK_V_ACTIVE to 720, .x_res to 480, .y_res to 720 and .cycle_time_ns to 37 I would expect to have a dot clock frequency of about 26.9 MHz. If I change the resolution again I would expect a different dot clock frequency insted on dot clock pin of the LCD panel I read always 25MHz.
Do you have any explanation about it?
Thanks very much!
Yes it can and it's very simple.
You only need to change the
#define DOTCLK_V_ACTIVE 600
and
static struct mxs_platform_fb_entry fb_entry = {
.name = "43wvf1g",
.x_res = 600,
.y_res = 800,
in drivers/video/mxs/lcd_43wvf1g.c file.
I've tested it and it works.
Hi Marco,
I have a imx28evk board with a Seiko 4.3" lcd panel. I have a question about the dot clock frequency of lcd panel.
If I set for example DOTCLK_V_ACTIVE to 480,DOTCLK_V_ACTIVE to 720, .x_res to 480, .y_res to 720 and .cycle_time_ns to 37 I would expect to have a dot clock frequency of about 26.9 MHz. If I change the resolution again I would expect a different dot clock frequency insted on dot clock pin of the LCD panel I read always 25MHz.
Do you have any explanation about it?
Thanks very much!