Can the cores interrupt each other in i.MX6? I don't see it in the reference manual.
解決済! 解決策の投稿を見る。
hi, you may refer to "uboot-imx/include/asm-arm/arch-mx6/mx6.h"
/* Cortex-A9 MPCore private memory region */
#define ARM_PERIPHBASE 0x00A00000
#define SCU_BASE_ADDR (ARM_PERIPHBASE)
#define IC_INTERFACES_BASE_ADDR (ARM_PERIPHBASE + 0x0100)
#define GLOBAL_TIMER_BASE_ADDR (ARM_PERIPHBASE + 0x0200)
#define PRIVATE_TIMERS_WD_BASE_ADDR (ARM_PERIPHBASE + 0x0600)
#define IC_DISTRIBUTOR_BASE_ADDR (ARM_PERIPHBASE + 0x1000)
hi Jim,
I may not get your point. ARM multiple-cores use the same interrupt controller, and it seems unable to interrupt specific CPU core by this controller.
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0407e/CCHDBEBE.html
Correct my previous reply. This register can meet the requirement.
[23:16] | CPUTargetList | When TargetList Filter = 0b00, defines the CPU interfaces the Distributor must send the interrupt to. Each bit of CPUTargetList[7:0] refers to the corresponding CPU interface, for example CPUTargetList[0] corresponds to CPU interface 0. Setting a bit to 1 sends the interrupt to the corresponding interface. |
//"arch/arm/common/gic.c"
508 #ifdef CONFIG_SMP
509 void gic_raise_softirq(const struct cpumask *mask, unsigned int irq)
510 {
511 unsigned long map = *cpus_addr(*mask);
512
513 /*
514 * Ensure that stores to Normal memory are visible to the
515 * other CPUs before issuing the IPI.
516 */
517 dsb();
518
519 /* this always happens on GIC0 */
520 writel_relaxed(map << 16 | irq, gic_data[0].dist_base + GIC_DIST_SOFTINT);
521 }
522 #endif
Could you tell what is the address of
register in the i.mx6q memory MAP?