Hi! All,
I want to set fb2 resolution same as fb0, here is my code(overrall):
------------------------
... ...
struct fb_var_screeninfo fbVar;
struct fb_var_screeninfo fb2_var;
int fb = open("/dev/fb0", O_RDWR, 0);
ioctl(fb, FBIOGET_VSCREENINFO, &fbVar);
int fb2 = open("/dev/fb2", O_RDWR, 0);
ioctl(fb2, FBIOGET_VSCREENINFO, &fb2_var);
memset(&fb2_var, 0x00, sizeof(fb_var_screeninfo));
memcpy(&fb2_var, &fbVar, sizeof(fb_var_screeninfo));
ioctl(fb2, FBIOPUT_VSCREENINFO, &fb2_var);
... ...
-----------------------
I konw fb0 resolution 1024x768,as following(command fbset):
mode "1024x768-60"
# D: 65.003 MHz, H: 48.365 kHz, V: 60.006 Hz
geometry 1024 768 1024 2304 16
timings 15384 160 24 29 3 136 6
rgba 5/11,6/5,5/0,0/0
endmode
But i get fb2 info as following:
fb2_var.xres = 1023
fb2_var.yres = 632 OR
fb2_var.xres = 856
fb2_var.yres = 610 etc.
I need your help
Thanks and best regards.
Not the approach you want, but this changes my /dev/fb2 resolution to 1024x768:
gst-launch-0.10 -e mfw_v4lsrc sensor-width=720 sensor-height=288 capture-width=720 capture-height=576 preview=true preview-width=1024 preview-height=768 fps-n=25 bg=true ! mfw_vpuencoder ! avimux name=mux ! filesink location=/mnt/usb1/PALfps25f.avi