Can't see USB Memory stick on MX28 EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't see USB Memory stick on MX28 EVK

738 Views
JayWilliamStubb
Contributor II

 I'm trying to see a USB Drive when it is connected to the USB Host port on the MX28 EVK board. I've been told by support that "sda1" should appear. This doesn't happen. I've tried loading my SD card with the L2.6.35 image (actually, it looks like the image is actually L2.6.31 when I'm programming the SD card even though I got it from L2.6.35_10.12.01_SDK_images_MX28.tar.gz file. Where can I pick up the correct image?) using both the MK_MX28_SD Script and the MFG Tool.

As far as the MFG Tool, I just changed the *.sb file. Do you have to change the rootfs.* file or other files as well? Can the SD cards be larger than 2G and can they be HC or higher speed card(s)?

Tags (1)
0 Kudos
Reply
2 Replies

668 Views
JayWilliamStubb
Contributor II

 I have this working now.

Maybe I didn't have something configured correctly in the kernel.

0 Kudos
Reply

668 Views
daiane_angolini
NXP Employee
NXP Employee

can you, please, share your dmesg?

anyone

0 Kudos
Reply