Can't see USB Memory stick on MX28 EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't see USB Memory stick on MX28 EVK

828 次查看
JayWilliamStubb
Contributor II

 I'm trying to see a USB Drive when it is connected to the USB Host port on the MX28 EVK board. I've been told by support that "sda1" should appear. This doesn't happen. I've tried loading my SD card with the L2.6.35 image (actually, it looks like the image is actually L2.6.31 when I'm programming the SD card even though I got it from L2.6.35_10.12.01_SDK_images_MX28.tar.gz file. Where can I pick up the correct image?) using both the MK_MX28_SD Script and the MFG Tool.

As far as the MFG Tool, I just changed the *.sb file. Do you have to change the rootfs.* file or other files as well? Can the SD cards be larger than 2G and can they be HC or higher speed card(s)?

标记 (1)
0 项奖励
回复
2 回复数

758 次查看
JayWilliamStubb
Contributor II

 I have this working now.

Maybe I didn't have something configured correctly in the kernel.

0 项奖励
回复

758 次查看
daiane_angolini
NXP Employee
NXP Employee

can you, please, share your dmesg?

anyone

0 项奖励
回复