Can't run iMX6Q DDR stress test binary

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't run iMX6Q DDR stress test binary

894 Views
sajjadahmed
Contributor II

Hi,

I'm trying to run the DDR stress test using the u-boot method on iMX6Q sabreSD board. Following the guide, I place the ddr-test-uboot-jtag-mx6dq.bin binary on the SD card and try to load it to the OCRAM but uboot refused to do this with the following error:

=> fatload mmc 2:1 0x00907000 ddr-test-uboot-jtag-mx6dq.bin
** Reading file would overwrite reserved memory **

The total size of the test binary is around 121K which means it shouldn't be having any problem sitting at 256K of OCRAM. I also tried the starting address of OCRAM 0x0090_0000 but no success, here are the complete steps I followed according to the guide.

U-Boot 2020.04-5.4.47-2.2.0+gffc3fbe7 (Nov 23 2020 - 10:42:56 +0000)

CPU:   i.MX6Q rev1.3 996 MHz (running at 792 MHz)
CPU:   Automotive temperature grade (-40C to 125C) at 40C
Reset cause: POR
Model: i.MX6 Quad SABRE Smart Device Board
Board: MX6-SabreSD
DRAM:  1 GiB
PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x21
MMC:   FSL_SDHC: 1, FSL_SDHC: 2, FSL_SDHC: 3
In:    serial
Out:   serial
Err:   serial
flash target is MMC:2
Net:   
Warning: ethernet@02188000 using MAC address from ROM
eth0: ethernet@02188000 [PRIME]
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot:  0 
=> dcache off
=> icache off
=> fatls mmc 2:1
 28908612   fitImage-a
   121880   ddr-test-uboot-jtag-mx6dq.bin

2 file(s), 0 dir(s)

=> fatload mmc 2:1 0x00907000 ddr-test-uboot-jtag-mx6dq.bin
** Reading file would overwrite reserved memory **
=> fatload mmc 2:1 0x00900000 ddr-test-uboot-jtag-mx6dq.bin 
** Reading file would overwrite reserved memory **
=> fatload mmc 2:1 0x00940000 ddr-test-uboot-jtag-mx6dq.bin
** Reading file would overwrite reserved memory **

 Kindly point what's the problem?

 

Sajjad

0 Kudos
Reply
2 Replies

735 Views
caioheitor_oliv
Contributor I

It worked for me, I was having the same problem. Now I could ran the DDR Stress Tool with no problems. Thank you

0 Kudos
Reply

872 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

This may be caused due to the fact that the u-boot from >= L5.4.24  checks if the load address is in a reserved area of memory for u-boot or not.

You may use the following commands, I used them on my side and it is working:

u-boot> dcache off; icache off; fatload mmc 2:1 0x12000000 ddr-test-uboot-jtag-mx6dq.bin; cp.b 0x12000000 0x00907000 0x20000; go 0x00907000

Please try it and let me know if this does not work.

Thank you,
Regards,
Aldo.