Hi All,
I'm a new user on RTnet and try to make Rtnet work on Freescale Sabre Lite iMX6Q board. But I got an issue, RTnet can't use rt_fec.ko module driver to register rt_eth0 even though non real time driver is disable.
I'm using:
Linux kernel 3.0.43 download from Xenomai git: http://git.xenomai.org/ipipe-gch.git/?h=ipipe-3.0-imx6q
Xenomai 2.6 download from http://git.xenomai.org/xenomai-2.6.git/
RTnet 0.9.13 download from http://rtnet.org/download.html
Please see my kernel configuration and boot log in attached file.
Xenomai is loaded:
Xenomai: hal/arm started.
Xenomai: scheduling class idle registered.
Xenomai: scheduling class rt registered.
Xenomai: real-time nucleus v2.6.3 (Lies and Truths) loaded.
Xenomai: debug mode enabled.
Xenomai: starting native API services.
Xenomai: starting POSIX services.
Xenomai: starting RTDM services. "
And FEC ethernet driver (non real-time driver) is loaded when kernel is booting
fec_enet_mii_bus: probed "
Xenomai is built following install guideline for ARM platform from Xenomai:
http://xenomai.org/installing-xenomai-2-x/
RTnet is built by below command, because SABRE Lite use FEC ethernet card with Micrel KSZ9021 Gigabit chip so I put "--enable-fec" in configure command to build real-time driver for FEC ethernet card:
Then
"make DESTDIR=/home/sonnguyen/rtnet-xenomai-rootfs install"
I also changed RT_DRIVER from default value to "rt_fec" in rtnet.conf.
After kernel is booted, I ran "./rtnet start" and got this:
"RTnet: initialising real-time networking
RT FEC Ethernet Driver
./rtnet: line 385: can't create /sys/bus/pci/drivers/rt_fec/bind: nonexistent directory
initializing loopback...
RTnet: registered rtlo
RTcap: real-time capturing interface
ifconfig: SIOCGIFFLAGS: No such device
ifconfig: SIOCGIFFLAGS: No such device
RTcfg: init real-time configuration distribution protocol
RTmac: init realtime media access control
RTmac/TDMA: init time division multiple access control mechanism
ioctl: No such device
ioctl: No such device
ioctl: No such device
ioctl: No such device
ioctl (add): No such device
ioctl (add): No such device
ioctl (add): No such device
ifconfig: SIOCGIFFLAGS: No such device
Waiting for all slaves...ioctl: No such device
ioctl: No such device "
Then I tried:
lspci: /sys/bus/pci/devices: No such file or directory
ac97 hid mdio_bus platform sdio spi
event_source i2c mmc scsi serio usb "
No pci directory under /sys/bus/. Then I thought because the script can't find the ethernet physical bus, it can't register rteth0.
Then I looked into rtnet script and did some minor change. In the script it requires physical ethernet device ID (mentioned in REBIND_RT_NICS), so I tried to find out what it is and got this when make eth0 up with non real-time driver:
PHY: 1:06 - Link is Up - 1000/Full "
I think 1:06 is my physical bus ID, then I change the code in rtnet from:
if [ -d /sys/bus/pci/devices/$dev/driver ]; then
echo $dev > /sys/bus/pci/devices/$dev/driver/unbind
fi
echo $dev > /sys/bus/pci/drivers/$RT_DRIVER/bind
done
To
echo 1:06 > /sys/bus/mdio_bus/drivers/Micrel\ KSZ9021\ Gigabit\ PHY/unbind
echo 1:06 > /sys/bus/platform/drivers/rt_fec/bind
And I tried again with "./rtnet start", this time I got this:
RT FEC Ethernet Driver
sh: write error: No such device
initializing loopback...
RTnet: registered rtlo
RTcap: real-time capturing interface
ifconfig: SIOCGIFFLAGS: No such device
ifconfig: SIOCGIFFLAGS: No such device
RTcfg: init real-time configuration distribution protocol
RTmac: init realtime media access control
RTmac/TDMA: init time division multiple access control mechanism
ioctl: No such device
ioctl: No such device
ioctl: No such device
ioctl: No such device
ioctl (add): No such device
ioctl (add): No such device
ioctl (add): No such device
ifconfig: SIOCGIFFLAGS: No such device
Waiting for all slaves...ioctl: No such device
ioctl: No such device
But it still said "No such device"
This is lsmod after I ran ./rtnet start
Module Size Used by Not tainted
tdma 25691 0
rtmac 9724 1 tdma
rtcfg 58071 0
rtcap 7151 0
rt_loopback 1279 2
rtpacket 6365 0
rtudp 10738 0
rt_fec 12742 0
rtipv4 29987 2 rtcfg,rtudp
rtnet 40746 9 tdma,rtmac,rtcfg,rtcap,rt_loopback,rtpacket,rtudp,rt_fec,rtipv4
rtlo Medium: Local Loopback
IP address: 127.0.0.1
UP LOOPBACK RUNNING MTU: 1500
Only rtlo is registered.
I also tried with kernel linux without non real-time FEC driver (please refer in another config file attached in this email), but still the same issue happened.
Do you have any idea how to solve this issue? I did many search but still can not figure out how to fix it.
Best Regards,
Nguyen Hung Son
Original Attachment has been moved to: kernel_config.zip
Original Attachment has been moved to: kernel_config_without_FEC.zip
Original Attachment has been moved to: rtnet_config.status.zip
Original Attachment has been moved to: rtnet.conf.zip