Can't login on Ubuntu rootfs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't login on Ubuntu rootfs

626件の閲覧回数
erikraynolds
Contributor III

Per https://community.nxp.com/docs/DOC-330147 I've installed Ubuntu rootfs. Unfortunately can't login. I do have "login screen" and got stuck on this screen. Is it possible to login directly without login screen (automatic login)?

Today I can't login through "login screen" either as root, or as via created user L:MyUser P:MyUser .

Does anybody have experience login with it?

Thank you.

0 件の賞賛
返信
1 返信

434件の閲覧回数
b36401
NXP Employee
NXP Employee

If there is some issue with logging without password I can suggest to try to set some password for root instead:
passwd -R /media/rootfs/ root

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信