Can't download hello world into M4 in the MCIMX8M-EVK eval board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't download hello world into M4 in the MCIMX8M-EVK eval board

1,331 Views
gsmgbl
Contributor IV

Hi there,

I followed doc "Getting Started with MCUXpresso SDK i.MX 8M Quad" and setup my IAR environment successfully, plus it complied with no error, see image below.

gilbertmlliu_0-1633041792099.png

Unfortunately, i couldn't download to the eval board and have the JLink driver message "Failed to get CPU status......", see image below.

gilbertmlliu_1-1633041868680.png

I checked my setup and couldn't find any problem or anything i missed, see the following images.

gilbertmlliu_2-1633041968927.pnggilbertmlliu_3-1633041997344.pnggilbertmlliu_4-1633042011860.pnggilbertmlliu_5-1633042023687.png

BTW, I opened two terminal to see the debug messages, i have the Linux side showing messages, but not the M4 side, see below.

gilbertmlliu_6-1633042168278.png

gilbertmlliu_7-1633042180743.png

I am using this SDK version "SDK_2_10_0_EVK-MIMX8MQ".

My goal is first try out a few samples project, such as hello world, mulitcore pingpong and string echo etc., eventually hope i can create messaging function through the remote processor messaging between A53 (Linux) and M4 (maybe RTOS, but not necessary).

Please advise if there is any tips and recommendation.

Thanks in advance!

Gilbert

 

 

Tags (3)
0 Kudos
Reply
5 Replies

1,300 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
Reply

1,286 Views
gsmgbl
Contributor IV

Hi Yuri,

Thanks for your info. In fact, I forgot to mention that i've got the 3rd party SDK already, you may see it from my environment image. Unfortunately, i still couldn't download the binary into the M4.

Do you have other suggestion?

Regards,

Gilbert

0 Kudos
Reply

1,282 Views
gsmgbl
Contributor IV

Hi Yuri,

I finally downloaded the binary into the M4 now.

I found that I have a later IAR version 8.50 available, somehow it was using the old version of IAR that causing the problem.

Regards,

Gilbert

1,314 Views
gsmgbl
Contributor IV

Hi there,

I am able to connect to the M4 core through the JLink commander, see below.

gsmgbl_0-1633108686560.png

But still having problem to download the hello world binary into the M4, see error message below.

gsmgbl_1-1633108784488.png

I followed this following page to check the boot switch.

https://www.nxp.com/document/guide/getting-started-with-the-mcimx8m-evk:GS-MCIMX8M-EVK

I also using the linux boot code and boot from SD card, Linux is booting up, but I still couldn't download binary into the M4.

Please advise. Thanks!

Gilbert

0 Kudos
Reply

1,313 Views
gsmgbl
Contributor IV

Here is the log from IAR while i download the hello world binary.

Fri Oct 01, 2021 10:18:57: IAR Embedded Workbench 8.50.1 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4\arm\bin\armproc.dll)
Fri Oct 01, 2021 10:18:57: Device "CORTEX-M4" selected.
Fri Oct 01, 2021 10:18:57: JLINK command: ProjectFile = C:\Users\GLIU\Desktop\iMX8\EVK\SDK_2_10_0_EVK-MIMX8MQ\boards\evkmimx8mq\demo_apps\hello_world\iar\settings\hello_world_debug.jlink, return = 0
Fri Oct 01, 2021 10:18:57: Device "CORTEX-M4" selected.
Fri Oct 01, 2021 10:18:57: DLL version: V6.62a, compiled Jan 31 2020 12:58:08
Fri Oct 01, 2021 10:18:57: Firmware: J-Link V9 compiled May 7 2021 16:26:12
Fri Oct 01, 2021 10:18:57: JTAG speed is initially set to: 32 kHz
Fri Oct 01, 2021 10:18:57: TotalIRLen = 4, IRPrint = 0x01
Fri Oct 01, 2021 10:18:57: JTAG chain detection found 1 devices:
Fri Oct 01, 2021 10:18:57: #0 Id: 0x5BA00477, IRLen: 04, CoreSight JTAG-DP
Fri Oct 01, 2021 10:18:57: Cannot determine DP version. Assuming DPv0
Fri Oct 01, 2021 10:18:57: Scanning AP map to find all available APs
Fri Oct 01, 2021 10:18:57: AP[5]: Stopped AP scan as end of AP map has been reached
Fri Oct 01, 2021 10:18:57: AP[0]: AHB-AP (IDR: 0x64770001)
Fri Oct 01, 2021 10:18:57: AP[1]: APB-AP (IDR: 0x44770002)
Fri Oct 01, 2021 10:18:57: AP[2]: JTAG-AP (IDR: 0x24760010)
Fri Oct 01, 2021 10:18:57: AP[3]: JTAG-AP (IDR: 0x001C0030)
Fri Oct 01, 2021 10:18:57: AP[4]: AHB-AP (IDR: 0x24770011)
Fri Oct 01, 2021 10:18:57: Iterating through AP map to find AHB-AP to use
Fri Oct 01, 2021 10:18:58: AP[0]: Skipped. No ROM table (AHB-AP ROM base: 0x00000000)
Fri Oct 01, 2021 10:18:58: AP[1]: Skipped. Not an AHB-AP
Fri Oct 01, 2021 10:18:58: AP[2]: Skipped. Not an AHB-AP
Fri Oct 01, 2021 10:18:58: AP[3]: Skipped. Not an AHB-AP
Fri Oct 01, 2021 10:18:58: AP[4]: Core found
Fri Oct 01, 2021 10:18:58: AP[4]: AHB-AP ROM base: 0xE00FF000
Fri Oct 01, 2021 10:18:58: CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)
Fri Oct 01, 2021 10:18:58: Found Cortex-M4 r0p1, Little endian.
Fri Oct 01, 2021 10:18:58: FPUnit: 6 code (BP) slots and 2 literal slots
Fri Oct 01, 2021 10:18:58: CoreSight components:
Fri Oct 01, 2021 10:18:58: ROMTbl[0] @ E00FF000
Fri Oct 01, 2021 10:18:58: ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7
Fri Oct 01, 2021 10:18:58: ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 003BB002 DWT
Fri Oct 01, 2021 10:18:58: ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 002BB003 FPB
Fri Oct 01, 2021 10:18:58: ROMTbl[0][3]: E0000000, CID: B105E00D, PID: 003BB001 ITM
Fri Oct 01, 2021 10:18:58: ROMTbl[0][5]: E0041000, CID: B105900D, PID: 000BB925 ETM
Fri Oct 01, 2021 10:18:58: ROMTbl[0][7]: E0043000, CID: B105900D, PID: 001BB908 CSTF
Fri Oct 01, 2021 10:18:58: ROMTbl[0][8]: E0044000, CID: B105900D, PID: 004BB906 CTI
Fri Oct 01, 2021 10:18:58: Reset: Halt core after reset via DEMCR.VC_CORERESET.
Fri Oct 01, 2021 10:18:58: Reset: Reset device via AIRCR.SYSRESETREQ.
Fri Oct 01, 2021 10:18:58: Reset: S_RESET_ST never gets cleared. CPU seems to be kept in reset forever.
Fri Oct 01, 2021 10:18:58: Reset: Using fallback: Reset pin.
Fri Oct 01, 2021 10:18:58: Reset: Halt core after reset via DEMCR.VC_CORERESET.
Fri Oct 01, 2021 10:18:58: Reset: Reset device via reset pin
Fri Oct 01, 2021 10:18:59: Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).
Fri Oct 01, 2021 10:18:59: Reset: Reconnecting and manually halting CPU.
Fri Oct 01, 2021 10:18:59: Cannot determine DP version. Assuming DPv0
Fri Oct 01, 2021 10:18:59: AP map detection skipped. Manually configured AP map found.
Fri Oct 01, 2021 10:18:59: AP[0]: MEM-AP (IDR: Not set)
Fri Oct 01, 2021 10:18:59: AP[1]: MEM-AP (IDR: Not set)
Fri Oct 01, 2021 10:18:59: AP[2]: MEM-AP (IDR: Not set)
Fri Oct 01, 2021 10:18:59: AP[3]: MEM-AP (IDR: Not set)
Fri Oct 01, 2021 10:18:59: AP[4]: AHB-AP (IDR: Not set)
Fri Oct 01, 2021 10:18:59: AP[4]: Core found
Fri Oct 01, 2021 10:18:59: AP[4]: AHB-AP ROM base: 0xE00FF000
Fri Oct 01, 2021 10:18:59: CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)
Fri Oct 01, 2021 10:18:59: Found Cortex-M4 r0p1, Little endian.
Fri Oct 01, 2021 10:18:59: Warning: CPU could not be halted
Fri Oct 01, 2021 10:18:59: Reset: Core did not halt after reset, trying to disable WDT.
Fri Oct 01, 2021 10:18:59: Reset: Halt core after reset via DEMCR.VC_CORERESET.
Fri Oct 01, 2021 10:18:59: Reset: Reset device via reset pin
Fri Oct 01, 2021 10:19:00: Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).
Fri Oct 01, 2021 10:19:00: Reset: Reconnecting and manually halting CPU.
Fri Oct 01, 2021 10:19:00: Cannot determine DP version. Assuming DPv0
Fri Oct 01, 2021 10:19:00: AP map detection skipped. Manually configured AP map found.
Fri Oct 01, 2021 10:19:00: AP[0]: MEM-AP (IDR: Not set)
Fri Oct 01, 2021 10:19:00: AP[1]: MEM-AP (IDR: Not set)
Fri Oct 01, 2021 10:19:00: AP[2]: MEM-AP (IDR: Not set)
Fri Oct 01, 2021 10:19:00: AP[3]: MEM-AP (IDR: Not set)
Fri Oct 01, 2021 10:19:00: AP[4]: AHB-AP (IDR: Not set)
Fri Oct 01, 2021 10:19:00: AP[4]: Core found
Fri Oct 01, 2021 10:19:00: AP[4]: AHB-AP ROM base: 0xE00FF000
Fri Oct 01, 2021 10:19:00: CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)
Fri Oct 01, 2021 10:19:00: Found Cortex-M4 r0p1, Little endian.
Fri Oct 01, 2021 10:19:00: Warning: CPU could not be halted
Fri Oct 01, 2021 10:19:01: Warning: CPU could not be halted
Fri Oct 01, 2021 10:24:15: IAR Embedded Workbench 8.50.1 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4\arm\bin\armproc.dll)

0 Kudos
Reply