I can't seem to debug my bootloader nor the linux kernel via JTAG. Both on my custom board as on the MXSabreSD. I'm using a j-link Base from Segger.
I have started the J-Link GDB Server with the the following command:
JLinkGDBServer -device MCIMX6S4 -scriptfile IMX6SoloX_Connect_CortexA9.JLinkScript -speed auto -ir
The output of the GDB server is as follows:
SEGGER J-Link GDB Server V6.10i Command Line Version
JLinkARM.dll V6.10i (DLL compiled Oct 25 2016 19:26:37)
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: yes
Generate logfile: off
Verify download: off
Init regs on start: on
Silent mode: off
Single run mode: off
Target connection timeout: 0 ms
------J-Link related settings------
J-Link Host interface: USB
J-Link script: IMX6SoloX_Connect_CortexA9.JLinkScript
J-Link settings file: none
------Target related settings------
Target device: MCIMX6S4
Target interface: JTAG
Target interface speed: auto
Target endian: littleConnecting to J-Link...
J-Link is connected.
Firmware: J-Link V10 compiled Sep 1 2016 18:29:58
Hardware: V10.10
S/N: 50102046
Feature(s): GDB
Checking target voltage...
Target voltage: 3.32 V
Listening on TCP/IP port 2331
Connecting to target...WARNING: At least one of the connected devices is not JTAG compliant (IEEE Std 1149.1, 7.1.1.d, IR-cells). (NumDevices = 4, NumBitsSet = 3)WARNING: At least one of the connected devices is not JTAG compliant (IEEE Std 1149.1, 7.1.1.d, IR-cells). (NumDevices = 4, NumBitsSet = 3)
WARNING: At least one of the connected devices is not JTAG compliant (IEEE Std 1149.1, 7.1.1.d, IR-cells). (NumDevices = 4, NumBitsSet = 3)
WARNING: At least one of the connected devices is not JTAG compliant (IEEE Std 1149.1, 7.1.1.d, IR-cells). (NumDevices = 4, NumBitsSet = 3)
J-Link found 4 JTAG devices, Total IRLen = 17
JTAG ID: 0x4BA00477 (Cortex-A9)
Connected to target
Whenever I try to connect with a remote session I get the following warnings:
Waiting for GDB connection...Connected to 127.0.0.1
Reading all registers
Read 4 bytes @ address 0x00000000 (Data = 0xE59FF01C)
WARNING: Failed to read memory @ address 0xFFFFFFFC
WARNING: Failed to read memory @ address 0x00000000
WARNING: Failed to read memory @ address 0xFFFFFFFC
WARNING: Failed to read memory @ address 0x00000000
WARNING: Failed to read memory @ address 0xFFFFFFFE
WARNING: Failed to read memory @ address 0xFFFFFFFC
WARNING: Failed to read memory @ address 0x00000000
WARNING: Failed to read memory @ address 0xFFFFFFFE
WARNING: Failed to read memory @ address 0xFFFFFFFC
WARNING: Failed to read memory @ address 0x00000000
WARNING: Failed to read memory @ address 0xFFFFFFFC
WARNING: Failed to read memory @ address 0x00000000
WARNING: Failed to read memory @ address 0xFFFFFFFC
WARNING: Failed to read memory @ address 0x00000000
WARNING: Failed to read memory @ address 0x00000000
WARNING: Failed to read memory @ address 0x00000000
The downloading goes well when I perform a load from the local gdb session. But I get the same warnings at the end.
When I try to run the executable I get the following on the server:
Starting target CPU...
ERROR: Could not start CPU core. (ErrorCode: -1)
I can't seem to find what I'm doing wrong. Can anybody help me with this problem?
An openocd solution is also ok as long as I can use GDB for debugging.
Best regards,
Jeroen van der Laan
解決済! 解決策の投稿を見る。
It seemed that the problem was with the GDB init script. A good tutorial can be found here:
It seemed that the problem was with the GDB init script. A good tutorial can be found here:
Hi Jeroen
for connection to i.MX6SX please try segger suggestions on
[SOLVED] Freescale IMX6SoloX support - J-Link/Flasher related - SEGGER Forum
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------