Hello,
I am trying to add fw_printenv and fw_setenv to my yocto build. I have added "u-boot-fw-utils" to IMAGE_INSTALL_append but it causes an error. Error messages are below.
I have tried to create the .config file manually inside of the uboot devshell using "make menuconfig" but it did not help.
Am i doing something wrong? Has anyone successfully built "u-boot-fw-utils" for imx6ull?
Best regards.
Yuce.
Error message:
ERROR: u-boot-fw-utils-1_2017.09-r0 do_compile: oe_runmake failed
ERROR: u-boot-fw-utils-1_2017.09-r0 do_compile: Function failed: do_compile (log file is located at ...8070)
| make -f ./Makefile silentoldconfig
| make -f ./scripts/Makefile.build obj=scripts/basic
| rm -f .tmp_quiet_recordmcount
| make -f ./scripts/Makefile.build obj=scripts/kconfig silentoldconfig
| mkdir -p include/config include/generated
| test -e include/generated/autoksyms.h || \
| touch include/generated/autoksyms.h
| scripts/kconfig/conf --silentoldconfig Kconfig
| ***
| *** Configuration file ".config" not found!
| ***
| *** Please run some configurator (e.g. "make oldconfig" or
| *** "make menuconfig" or "make xconfig").
| ***
| scripts/kconfig/Makefile:46: recipe for target 'silentoldconfig' failed
| make[2]: *** [silentoldconfig] Error 1
| Makefile:478: recipe for target 'silentoldconfig' failed
| make[1]: *** [silentoldconfig] Error 2
| make: *** No rule to make target 'include/config/auto.conf', needed by 'include/config/uboot.release'. Stop.
| ERROR: oe_runmake failed
Hi Yüce kürüm
Along with the above solution provided by Wigros you can also try make mrproper command inside the u-boot devshell,it will help you to solve your errors.
Let us know in case of any concern
Regards,
Karan Gajjar
Hi,
I tested it just now , follow the steps below, please!
# cd imx-release-bsp
# gedit .build/conf/local.conf
add the line:
IMAGE_INSTALL_append += " u-boot-fw-utils" # a space character must be used before "u-boot-fw-utils".
save and exit.
# source setup-environment build
# bitbake u-boot-fw-utils -c compile
# bitbake u-boot-fw-utils -c install
Then succeeded.
Have a nice day!
BR
Weidong