Hello,
I am trying to get kernel 3.7-rc1 running on my mx28evk without much luck.
I get to this point "Uncompressing Kernel Image ... OK " and then nothing.
I have set 'console=ttyAMA0' per other posts describing the same behavior, with no luck.
So, could someone please post a 3.x kernel .config file for a working linux 3.x mx28evk boot so I can see if I have missed something else ?
FWIW, the stock fsl 2.6.35 kernel boots fine.
Thanks for any help.
-Randy
解決済! 解決策の投稿を見る。
You should use mxs_defconfig.
make mxs_defconfig.
Regards,
Fabio Estevam
Thanks Fabio.
Yes, I was using mxs_defconfig.
I am now using buildroot to build my kernel and rootfs and can successfully boot my board with kernel 3.7-rc1 .
I really like buildroot and will use it for my kernel and rootfs builds moving forward.
Thanks for you help!
-Randy