I have got a I.MX 6Quad SABRE board, then I want to download the Linux system with the Mfgtools-Rel-1.1.0_121218_MX6Q_UPDATER via the USB OTG , but I can not successfully download into the board.It stays at the state as the following picture.
The board I have set as fllows:
BOOT_MODE[1:0] = 10
BT_C FG1_7 BT_C FG1_6 B T_C FG1_5 BT_C FG1_4 :0011
BT_C FG2_6 BT_C FG2_5 BT_C FG2_4 B T_C FG2_3 :0000
I do not know if the setting it right .
the image ,u-boot and rootfs is from the freescale.com ( L3.0.35_4.1.0_130816_images_MX6).
已解决! 转到解答。
HI xiaobin
please try with MFG Tool from i.MX6DQ product page: i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale
IMX_6DQ_MFG_TOOL : Tool and documentation for downloading OS images to the i.MX 6Quad and i.MX6Dual.
Size (K): 75779 Format: gz Rev #: L3.0.35_4.1.0 Modified: 9/5/2013
also one needs to remove SD card, so board enters Serial Downloader mode.
Please check sect.4.1 How to Enter Serial Download Mode for MFGTool,
Chapter 6 Downloading Images by Using MFGTool attached Linux User Guide.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI xiaobin
please try with MFG Tool from i.MX6DQ product page: i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale
IMX_6DQ_MFG_TOOL : Tool and documentation for downloading OS images to the i.MX 6Quad and i.MX6Dual.
Size (K): 75779 Format: gz Rev #: L3.0.35_4.1.0 Modified: 9/5/2013
also one needs to remove SD card, so board enters Serial Downloader mode.
Please check sect.4.1 How to Enter Serial Download Mode for MFGTool,
Chapter 6 Downloading Images by Using MFGTool attached Linux User Guide.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov
I have download the i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf and IMX_6DQ_MFG_TOOL as your answer ,but the i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf just tell me how to config the sw6 after I have download the image int the EMMC.Now ,I can not download the image into the emmc,I do not know if it is what I config the sw6 and bootmod iare wrong or there is something wrong with my board .
I have config the sw6 (1 to 8) as 00110000 when download the image into the emmc;the bootmode[1:0] as 10.
Can you tell me if Ihave config the board correctlly?