Hi all ( it's me again....),
I am trying to burn the image to eMMC memory on our custom board based off sabreSD using MFGToolV2 4.15-2.0.0 , but i am not able to start the initrd filesystem to start the partitioning process. When i try, i get the following error:
Wrong Ramdisk Image Format
Ramdisk image is corrupt or invalid
I have build u-boot, kernel and initramfs (in cpio.gz.u-boot format) for the mfg tool using bitbake.
( we use imx BSP krogoth 2.0GA , kernel 4.1.15 )
For u-boot:
CONFIG_ENV_IS_NOWHERE
CONFIG_IMAGE_FORMAT_LEGACY
are defined.
I can start u-boot usng the MFGTool, and i can start the kernel if i do
bootz 0x12000000 | - | 0x18000000
kernel addr | skip initrd | device tree blob addr
And obviously it crashes as it can't find the ramdisk fs.
Below is my ucl.xml for this:
<LIST name="RamFS" desc="Test ram fs">
<CMD state="Bootstrap" type="boot" body="BootStrap" file ="bootstrap/u-boot-mfgtool.imx" ifdev="MX6D">Loading U-boot</CMD>
<CMD state="BootStrap" type="load" file="bootstrap/zImage_mfgtool" address="0x12000000"
loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev"MX6D">Loading Kernel.</CMD>
<CMD state="BootStrap" type="load" file="bootstrap/mfgtool-initramfs" address="0x12C00000"
loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev="MX6D">Loading Initramfs.</CMD>
<CMD state="BootStrap" type="load" file="bootstrap/imx6dl.dtb" address="0x18000000"
loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev="MX6D">Loading device tree.</CMD>
<CMD state="BootStrap" type="jump" > Jumping to OS image. </CMD>
<LIST/>
Looking at the code in image.c, it seems that the function that checks the initramdisk magic number fails:
https://lxr.missinglinkelectronics.com/uboot/include/image.h#L818static inline int image_check_magic(const image_header_t *hdr) { return (image_get_magic(hdr) == IH_MAGIC); }
However, when i open my initramdisk binary, the first 4 bytes actually match the expected magic number (which is: )
https://lxr.missinglinkelectronics.com/uboot/include/image.h#L309#define IH_MAGIC 0x27051956
And so, i am really confused. Since i can start kernel, the MFGTool seems to load things properly into RAM.
But then again, when i check the 0x12C00000 address with the md tool, it doesn't look like what i would expect.
Any pointers ? Thanks....
解決済! 解決策の投稿を見る。
Whooops nevermind, found the typo in my ucl.xml.....
<CMD state="BootStrap" type="load" file="bootstrap/zImage_mfgtool" address="0x12000000"
loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev"MX6D">Loading Kernel.</CMD>
Whooops nevermind, found the typo in my ucl.xml.....
<CMD state="BootStrap" type="load" file="bootstrap/zImage_mfgtool" address="0x12000000"
loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev"MX6D">Loading Kernel.</CMD>