Can not download imgs using mfgtools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not download imgs using mfgtools

759 Views
sunzhangyang
Contributor I

          I do a board with imx6ull myself, but i can not download imgs using mfgtools , so i want to know how to do when download imgs firstly.   I must use jlink the firstly downlod? 

        thanks

Labels (1)
0 Kudos
Reply
4 Replies

671 Views
sunzhangyang
Contributor I

thanks for you reply ,igor 

0 Kudos
Reply

671 Views
sunzhangyang
Contributor I

hi igorpadykov,

     PC Jump to Boot ROM if configured as download mode or empty boot device, so how to enter download mode for imx6ull and is my custom board a empty boot device when burning the firmware using Mfgtool firstly?

thanks

0 Kudos
Reply

671 Views
igorpadykov
NXP Employee
NXP Employee

please look at Boot Chapter of i.MX6ULL Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf 

Best regards
igor

0 Kudos
Reply

671 Views
igorpadykov
NXP Employee
NXP Employee

Hi sun

for mfg tools usage one can look at presentation

AMF-ACC-T1652 

for custom board first it is necessary to run ddr test

i.MX6/7 DDR Stress Test Tool V2.70 

then rebuild mfg tools firmware, it is described in linux documentation on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply