Can not build jack into recipe

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can not build jack into recipe

ソリューションへジャンプ
10,182件の閲覧回数
dougschwanke
Contributor IV

I can "bitbake jack" without any errors, but when I add jack to my recipe, I get an error that jack not found in the base feeds.  Is jack missing from the imx6qsabresd feed?

build$ bitbake jack

WARNING: Unable to get checksum for linux-boundary SRC_URI entry defconfig: file could not be found#########################################  | ETA:  00:00:00

Parsing recipes: 100% |#######################################################################################################################| Time: 00:00:56

Parsing of 1340 .bb files complete (0 cached, 1340 parsed). 1732 targets, 77 skipped, 0 masked, 0 errors.

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION        = "1.20.0"

BUILD_SYS         = "x86_64-linux"

NATIVELSBSTRING   = "Ubuntu-12.04"

TARGET_SYS        = "arm-poky-linux-gnueabi"

MACHINE           = "imx6qsabresd"

DISTRO            = "poky"

DISTRO_VERSION    = "1.5"

TUNE_FEATURES     = "armv7a vfp neon callconvention-hard cortexa9"

TARGET_FPU        = "vfp-neon"

meta             

meta-yocto        = "(nobranch):faf8f8660fae26a14578738b642fdeb08bcb9d54"

meta-oe           = "(nobranch):513e7ca20ddd0a5c3b649bf292a67c3e0473d3a8"

meta-fsl-arm      = "(nobranch):520339d3266bfd07bb2e593f70489efe4d98baa2"

meta-fsl-arm-extra = "(nobranch):b17d250c7f53a84855fd9a364a996ac5503c7693"

meta-fsl-demos    = "(nobranch):cd6275042cdd2d87490521f6cbeb65972ed37a66"

meta-test           = "<unknown>:<unknown>"

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

NOTE: Tasks Summary: Attempted 859 tasks of which 846 didn't need to be rerun and all succeeded.

Summary: There was 1 WARNING message shown.

test-image.bb:

COMMON_INSTALL = " \

    base-files \

    base-passwd \

    busybox \

    ${@base_contains("MACHINE_FEATURES", "systemd", "${SYSTEMD_INSTALL}", "${SYSV_INSTALL}", d)} \

    packagegroup-base \

    jack \

...

build$ bitbake test-image

Loading cache: 100% |#########################################################################################################################| ETA:  00:00:00

Loaded 1733 entries from dependency cache.

Parsing recipes: 100% |#######################################################################################################################| Time: 00:00:00

Parsing of 1340 .bb files complete (1339 cached, 1 parsed). 1732 targets, 77 skipped, 0 masked, 0 errors.

NOTE: Resolving any missing task queue dependencies

NOTE: multiple providers are available for jpeg (jpeg, libjpeg-turbo)

NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg

NOTE: multiple providers are available for jpeg-native (jpeg-native, libjpeg-turbo-native)

NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg-native

Build Configuration:

BB_VERSION        = "1.20.0"

BUILD_SYS         = "x86_64-linux"

NATIVELSBSTRING   = "Ubuntu-12.04"

TARGET_SYS        = "arm-poky-linux-gnueabi"

MACHINE           = "imx6qsabresd"

DISTRO            = "poky"

DISTRO_VERSION    = "1.5"

TUNE_FEATURES     = "armv7a vfp neon callconvention-hard cortexa9"

TARGET_FPU        = "vfp-neon"

meta             

meta-yocto        = "(nobranch):faf8f8660fae26a14578738b642fdeb08bcb9d54"

meta-oe           = "(nobranch):513e7ca20ddd0a5c3b649bf292a67c3e0473d3a8"

meta-fsl-arm      = "(nobranch):520339d3266bfd07bb2e593f70489efe4d98baa2"

meta-fsl-arm-extra = "(nobranch):b17d250c7f53a84855fd9a364a996ac5503c7693"

meta-fsl-demos    = "(nobranch):cd6275042cdd2d87490521f6cbeb65972ed37a66"

meta-test           = "<unknown>:<unknown>"

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

ERROR: Function failed: do_rootfs (log file is located at /media/work/dora/fsl-community-bsp/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/test-image/0.0+cvs20600815-r1/temp/log.do_rootfs.9775)

ERROR: Logfile of failure stored in: /media/work/dora/fsl-community-bsp/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/test-image/0.0+cvs20600815-r1/temp/log.do_rootfs.9775

Log data follows:

| DEBUG: Executing python function rootfs_process_ignore

| DEBUG: Python function rootfs_process_ignore finished

| DEBUG: Executing python function rootfs_runtime_mapping

| DEBUG: Python function rootfs_runtime_mapping finished

| DEBUG: Executing shell function do_rootfs

| Note: configuring RPM platform settings

| Note: configuring RPM system provides

| Note: configuring RPM DB settings

| Note: configuring Smart settings

|

| Note: adding Smart channel imx6qsabresd (65)

|

| Note: adding Smart channel cortexa9hf_vfp_neon_mx6 (60)

|

| Note: adding Smart channel cortexa9hf_vfp_neon (55)

| Note: adding Smart channel all (10)

| Note: configuring RPM cross-install scriptlet_wrapper

|

| Updating cache...               ######################################## [100%]

|

| Saving cache...

|

| Error: jack not found in the base feeds (imx6qsabresd cortexa9hf-vfp-neon-mx6 cortexa9hf-vfp-neon cortexa9hf-vfp armv7ahf-vfp-neon armv7ahf-vfp armv6hf-vfp armv5ehf-vfp armv5hf-vfp noarch any all).

| WARNING: exit code 1 from a shell command.

| ERROR: Function failed: do_rootfs (log file is located at /media/work/dora/fsl-community-bsp/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/test-image/0.0+cvs20600815-r1/temp/log.do_rootfs.9775)

ERROR: Task 7 (/media/work/dora/fsl-community-bsp/sources/meta-test/recipes-qt/images/test-image.bb, do_rootfs) failed with exit code '1'

NOTE: Tasks Summary: Attempted 4447 tasks of which 4445 didn't need to be rerun and 1 failed.

No currently running tasks (4446 of 4448)

Summary: 1 task failed:

  /media/work/dora/fsl-community-bsp/sources/meta-test/recipes-qt/images/test-image.bb, do_rootfs

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

build$

ラベル(1)
タグ(1)
1 解決策
2,373件の閲覧回数
dougschwanke
Contributor IV

I was able to get the correct answer from the [meta-freescale] mail group.

On Thu, Oct 31, 2013 at 1:15 PM, Doug Schwanke <doug.schwanke@firstviewconsultants.com> wrote:

> I can "bitbake jack" without any errors, but when I add “jack” to my recipe, I get an error that jack not found in the base feeds.

>

> Is “jack” missing from the imx6qsabresd feed or do I need to add some kind of depends?

Neither; this is common for people starting to Yocto to make this mistake. Basically you need to check the binary packages it builds.

When you do:

$: bitbake jack

You are saying ... hey bitbake, please process jack recipe. This has no direct relation to the binaries you get as result.

When you add something in IMAGE_INSTALL or similar, you are asking for the image to install the /binary/. For jack case, the binaries are:

http://git.openembedded.org/meta-openembedded/tree/meta-oe/recipes-multimedia/jack/jack_0.121.0.bb?h...

Most probably, you're looking for jack-server binary.

=========================

Adding the following line to my recipe fixed the issue:

libjack jack-server jack-utils \

元の投稿で解決策を見る

0 件の賞賛
10 返答(返信)
2,374件の閲覧回数
dougschwanke
Contributor IV

COMMON_INSTALL is included as part of IMAGE_INSTALL.  I used qte-in-use-image from the meta-fsl-demos as my template since I need multiple ways to build my image.

IMAGE_INSTALL is actually in my test-common.inc file.  All of my other packages that I include into COMMON_INSTALL work.  jack is the exception. 

My actual test-image.bb look like this:

require test-common.inc

IMAGE_INSTALL = " \

    ${COMMON_INSTALL} \

    \

    ${QT_DEMOS} \

    qt-in-industrial-embedded-smarthome-e \

    pciutils \

    usbutils \

    alsa-utils \

"

The error message "Error: jack not found" indicates to me it was parsed by bitbake.

0 件の賞賛
2,374件の閲覧回数
LeonardoSandova
Specialist I

NOt sure what is going on. Last check: do a search under the sources folder and filter the recipe (find | grep jack). Then make sure the layer is on the bblayers.conf file.

Leo

0 件の賞賛
2,374件の閲覧回数
dougschwanke
Contributor IV

I was able to get the correct answer from the [meta-freescale] mail group.

On Thu, Oct 31, 2013 at 1:15 PM, Doug Schwanke <doug.schwanke@firstviewconsultants.com> wrote:

> I can "bitbake jack" without any errors, but when I add “jack” to my recipe, I get an error that jack not found in the base feeds.

>

> Is “jack” missing from the imx6qsabresd feed or do I need to add some kind of depends?

Neither; this is common for people starting to Yocto to make this mistake. Basically you need to check the binary packages it builds.

When you do:

$: bitbake jack

You are saying ... hey bitbake, please process jack recipe. This has no direct relation to the binaries you get as result.

When you add something in IMAGE_INSTALL or similar, you are asking for the image to install the /binary/. For jack case, the binaries are:

http://git.openembedded.org/meta-openembedded/tree/meta-oe/recipes-multimedia/jack/jack_0.121.0.bb?h...

Most probably, you're looking for jack-server binary.

=========================

Adding the following line to my recipe fixed the issue:

libjack jack-server jack-utils \
0 件の賞賛
2,374件の閲覧回数
LeonardoSandova
Specialist I

Great! Also, one way to know the REAL name, is to bake the recipe, then check the subfolders of tmp/work/.../jack/../../packages-split. Most of the times you find the jack-dev, -locale and in the case of jack, you may find the -server or -utils one. Just a tip for the future. So just add the jack-* in your local.conf.

Leo

0 件の賞賛
2,374件の閲覧回数
craigdenson
Contributor II

I'm trying to create an SDK for an image that uses jack. when I  bitbake my-image, everything is happy, but when I enter bitbake my-image -c populate_sdk, it complains with

|  * satisfy_dependencies_for: Cannot satisfy the following dependencies for jack-dev:

|  *     jack (= 0.121.0-r0) *

|  * opkg_install_cmd: Cannot install package jack-dev.

When I look at tmp/work/../jack/../packages-split I see:

  drwx------ 1 dcd dcd   0 Jan 28 13:56 jack

  drwx------ 1 dcd dcd   6 Jan 28 13:56 jack-dbg

  drwx------ 1 dcd dcd   6 Jan 28 13:56 jack-dev

  drwx------ 1 dcd dcd   6 Jan 28 13:56 jack-doc

  drwx------ 1 dcd dcd   0 Jan 28 13:56 jack-locale

  drwx------ 1 dcd dcd   6 Jan 28 13:56 jack-server

  -rw-r--r-- 1 dcd dcd  38 Jan 28 13:56 jack-server.shlibdeps

  drwx------ 1 dcd dcd   0 Jan 28 13:56 jack-staticdev

  drwx------ 1 dcd dcd   6 Jan 28 13:56 jack-utils

  -rw-r--r-- 1 dcd dcd 130 Jan 28 13:56 jack-utils.shlibdeps

  drwx------ 1 dcd dcd   6 Jan 28 13:56 libjack

  -rw-r--r-- 1 dcd dcd  67 Jan 28 13:56 libjack.shlibdeps

but, the jack directory is empty, and if I look in the deploy-ipks/cortexa9hf-vfp-neon directory I see this:

  -rw-r--r-- 2 dcd dcd 1010372 Jan 28 13:56 jack-dbg_0.121.0-r0_cortexa9hf-vfp-neon.ipk

  -rw-r--r-- 2 dcd dcd   32324 Jan 28 13:56 jack-dev_0.121.0-r0_cortexa9hf-vfp-neon.ipk

  -rw-r--r-- 2 dcd dcd  177666 Jan 28 13:56 jack-doc_0.121.0-r0_cortexa9hf-vfp-neon.ipk

  -rw-r--r-- 2 dcd dcd   10234 Jan 28 13:56 jack-server_0.121.0-r0_cortexa9hf-vfp-neon.ipk

  -rw-r--r-- 2 dcd dcd   89390 Jan 28 13:56 jack-utils_0.121.0-r0_cortexa9hf-vfp-neon.ipk

  -rw-r--r-- 2 dcd dcd  181590 Jan 28 13:56 libjack_0.121.0-r0_cortexa9hf-vfp-neon.ipk

Something changed in my build that made this stop working but I don't know how to resolve it

0 件の賞賛
2,374件の閲覧回数
LeonardoSandova
Specialist I

can you create a higher version recipe and see if that fixes it?

0 件の賞賛
2,374件の閲覧回数
craigdenson
Contributor II

I was not able to find or alter an image that included jack that would create an SDK. I ended up removing it from our image. Note that it builds and installs normally, it's only the populate_sdk that fails.

0 件の賞賛
2,374件の閲覧回数
LeonardoSandova
Specialist I

can you add this into the jack recipe?

ALLOW_EMPTY_${PN}-dev = "1"

0 件の賞賛
2,374件の閲覧回数
craigdenson
Contributor II

Thanks for the pointer and sorry for the long delay. The jack recipe is sort of messed up, because it doesn't create a jack package. Your suggestion failed with this:

| Collected errors:

|  * satisfy_dependencies_for: Cannot satisfy the following dependencies for jack-dev:

|  *     jack (= 0.121.0-r0) *

|  * opkg_install_cmd: Cannot install package jack-dev.

However, changing it to

ALLOW_EMPTY_${PN} = "1"

at least allows the populate_sdk task to complete. thanks.

2,374件の閲覧回数
LeonardoSandova
Specialist I

isn't it IMAGE_INSTALL instead of COMMON_INSTALL?

Leo

0 件の賞賛