Can imx6 solox supports dual independent display?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can imx6 solox supports dual independent display?

675 Views
mohsengh
Contributor III

Hello Dears

my question is:

Can imx6 solox supports dual independent display? for example, can i use LCDIF1 as parallel lcd out and use LCDIF2 as video encoder interface in DVI mode?

is it possible to show two independent in such a configuration?

As we know solox has two LCDIF and 3 possible digital video output (two parrallel and on shared LVDS).

best regards

lcdif.png

0 Kudos
2 Replies

402 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Yes, it is possible to use both LCDIFs independently.

   Also, please look at the following :

 

https://community.nxp.com/message/636749 

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

402 Views
mohsengh
Contributor III

Dear Yuri

Thanks for your fast reply.

have a great day too.

0 Kudos