Can i use the LCD mudoule of imx233 EVK to imx233 with LQFP?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i use the LCD mudoule of imx233 EVK to imx233 with LQFP?

532 Views
stevenshan
Contributor II

I think  it is ok,LCD  only work with 8bit mode,is right?

Labels (1)
0 Kudos
2 Replies

407 Views
igorpadykov
NXP Employee
NXP Employee

Hi steven

i.MX23 EVK uses WQVGA LMS430 LCD Panel 4.3” Samsung display supporting

parallel 24bit RGB Interface with  DE(Data Enable) & SYNC mode,  Vsync, Hsync, DOTCLK signals.

While LQFP option supports 8 bits of LCD interface with modes:

8-bit serial RGB mode

ITU-R/BT.656 8-bit+clock mode

8-bit system mode

So seems it can not be used with i.MX23 EVK LCD.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

407 Views
stevenshan
Contributor II

igor

you are great ! thanks.

0 Kudos