Can M40 use ADMA_UART3 directly?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can M40 use ADMA_UART3 directly?

438 次查看
tiebing_guo
Contributor I

Dear Sirs

We are using android_p9.0.0_1.0.2-auto-beta release on IMX8QXP MEK board.

As the IMX8DQXPRM.pdf doc 12.5 shows the M40 LPUART supports to CTS&RTS for HW  stream control.

But I can't find M4_UART0 CTS or RTS define in the M40 SDK, could you please guide us where is it ? and  is there any demo code about it ?

On the IMX8QXP MEK board , only UART3's CTS&RTS pin are used as CTS、RTS function for BT UART,

is it possible the M40 to use the UART3 port directly in some situation?  Such as M40 to communicate with BT chip before A Core launch.

Thank you very much~

0 项奖励
1 回复

371 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

The i.MX8QXP is still on preproduction, so, no additional information/support could be provided yet. In case of having doubts, please refer with your Sales/FAE.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 项奖励