Can Imx6 solo boots up using Raw Nand Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can Imx6 solo boots up using Raw Nand Flash

710 Views
adityanagal
Contributor III

Hi 

I am working over the Imx6 solo based target board. In my design , Raw Nand is connected to IMX6 solo over GPMI interface. My questions are :

1. Can Imx6 solo boot from Raw Nand flash.

2. whats the difference  in booting from OneNand Flash  and Raw Nand Flash.

3. Can we program uboot over Raw Nand flash using Jtag programmer. 

Please suggest.

Regards , 

Aditya Nagal

0 Kudos
2 Replies

437 Views
Yuri
NXP Employee
NXP Employee

Hello,

 Please look at my comments below.

> 2. whats the difference  in booting from OneNand Flash  and Raw Nand Flash.

OneNAND has general purpose SRAM-like interface and it treated as NOR.

Raw NAND has different interface and is supported, using i.MX6 GPMI.  

> 3. Can we program uboot over Raw Nand flash using Jtag programmer. 

  Please refer to https://community.nxp.com/thread/450978 

Regards,

Yuri.

0 Kudos

437 Views
b36401
NXP Employee
NXP Employee

Actually i.MX6S can boot from raw nand flash.
However it requires many changes in kobs-ng and MFGtool.

Please create a technical case:
https://community.nxp.com/thread/381898

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos