Hello.
I am a beginner with i.mx8m mini. I am woking with variscite's var-imx8mm-dart evm board(with i.mx8m mini).
I want to use opencv with opencl. but, the opencl sample code is not working.
the sample executable is "/opt/viv_samples/cl11/UnitTest/clinfo". and other samples also failed.
root@imx8mm-var-dart:/opt/viv_samples/cl11/UnitTest# ./clinfo >>>>>>>> ./clinfo Starting... Available platforms: 1 Platform ID: 0 CL_PLATFORM_NAME: Vivante OpenCL Platform CL_PLATFORM_PROFILE: EMBEDDED_PROFILE CL_PLATFORM_VERSION: OpenCL 1.2 V6.2.4.p4.190076 CL_PLATFORM_VENDOR: Vivante Corporation CL_PLATFORM_EXTENSIONS: cl_khr_icd !!! Error # -30 at line 200 , in file main.cpp !!! !!! Exiting...
I built the image with "$bitbake fsl-image-gui".
let me know to use the opencl library?
Hello.
I have the same error on my IMX8M MINI EVK board.
!!! OpenCL and OpenVX are not supported in the IMX8M MINI !!!
I hope my post saves time for people with the same clinfo error.
Have a nice day
Hello Jaechul,
The error 30 means CL_INVALID_VALUE, that you need to compile the demos before use it. Or you are using it as invalid element.
Regards