Can I use SDMA for transferring memory to PCI space?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I use SDMA for transferring memory to PCI space?

ソリューションへジャンプ
847件の閲覧回数
hiromichimatsum
Contributor II

Dear all,


I'm developing the pci device driver on i.MX6Q.

The pci device doesn't have a DMA Controller.

So, I'd like to use SDMA in i.MX6Q.

What I want is to transfer memory to PCI space.

I don't know which script to use, though I read the i.MX6 reference manual.

Then I tried to use "Memory To Memory" script.

The execution was succeeded, but the data were not transferred at all to PCI space.

Can I use SDMA for transferring memory to PCI space?

What script is suitable for in this case?

Best regards,

Hiromichi

ラベル(1)
0 件の賞賛
返信
1 解決策
703件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Since the memory space for the PCI it is not part of the memory map of the SDMA it is not possible. To have an script from memory to PCI.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
704件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Since the memory space for the PCI it is not part of the memory map of the SDMA it is not possible. To have an script from memory to PCI.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信