When running CTS test android.security.cts.StagefrightTest we are getting an "Fatal signal 11 (SIGSEGV), code 1" error. We are running android 5.1.1 with the patches for BUG-21443020 added. The problem seams to occur when VPU frame memory is being freed. See attached Log. What could be the problem?
Original Attachment has been moved to: Log.txt.zip
解決済! 解決策の投稿を見る。
Hello
I apologize for the late answer. I do not know if you still have a problem.
Unfortunately, there are reports that CTS test android.security.cts.StagefrightTest failed. There is a "Fatal signal 11 (SIGSEGV), code 1" error:
"09-26 11:54:54.089 169 169 I DEBUG : signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr 0xb5000000:"[i.MX6Q][Android L5.1.1]CTS test failed: android.security.cts.StagefrightTest
As soon as the I can find a solution, I will let you know.
Best Regards,
Diego.
Hi
The problem was solved with the patch from Ankit Patel at NXP. So there is no longer an issue.
Regards
/Björn Qvarnström
I am glad that the problem was solved.
However, is there a possibility, that you can share to us the patch?
This is because, if there are further problems of this issue. The patch could be a solution.
Best regards,
Diego.