I'm running on a iMX6Q Sabre Lite board.
For Building the imx6q-sabrelite.dtb file should be used the following files (imx6q-sabrelite.dts, imx6q.dtsi, imx6qdl.dtsi, imx6ql-sabrelite.dtsi and so on)
In the file arch/arm/boot/dts/imx6q.dtsi, particularly, are listed the CPU scaling operating points:
cpu0: cpu@0 {
compatible = "arm,cortex-a9";
device_type = "cpu";
reg = <0>;
next-level-cache = <&L2>;
operating-points = <
/* kHz uV */
1200000 1275000
996000 1250000
852000 1250000
792000 1175000
396000 975000
So these should be as far as I understood the scaling operating points passed from the bootloader to the kernel.
Am I right?
However, when I run the following command on both Yocto Linux and Android 5.1.1:
cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_available_frequencies
I get only these available scaling operating points:
396000 792000 996000
why are the 852000 and 1200000 frequencies not included in the CPU scaling policy?
Thank you in advance!
已解决! 转到解答。
Hi Francesco
this depends on frequency grade (can be read from fuse SPEED_GRADING[5:4]):
for example 1.2GHz part: MCIMX6Q5EYM12AC, MCIMX6Q6AVT08AC - 852MHz
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Francesco
this depends on frequency grade (can be read from fuse SPEED_GRADING[5:4]):
for example 1.2GHz part: MCIMX6Q5EYM12AC, MCIMX6Q6AVT08AC - 852MHz
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------