Hi,
My target is imx8quadmax mek.
I am running linux - imx-4.14.98-2.0.0_ga as dom0 and android- imx-p9.0.0_2.1.0-auto-ga as domU on xen - imx-xen version 4.11 as per the virtualization guide.
imx-lpi2c 58246000.i2c: can't get irq number
[ 10.040053] Failed power operation on resource 322 sc_err 4
[ 10.046105] imx8qm-pinctrl passthrough:iomuxc: pin_config_set op failed for pin 77
[ 10.046141] ov5640_mipi_v3 5-003c: Error applying setting, reverse things back
[ 10.046347] imx8qm-pinctrl passthrough:iomuxc: pin_config_set op failed for pin 77
[ 10.046363] ov5640_mipi_v3 5-003c: Error applying setting, reverse things back
[ 10.046382] ov5640_mipi_v3 5-003c: setup pinctrl failed
[ 10.046404] ov5640_mipi_v3: probe of 5-003c failed with error -5
If someone has succeeded in passthrough the mipi_csi1 camera to the android domU,
Please help me to solve the issue.