I'm using CAAM through Linux Crypto API as shown in kernel source tree crypto/tcrypt.c in a kernel module.
See the code segment below. I've changed the test_acipher_speed taken from tcrypt.c in my kernel module implementation to use BUFFSIZE instead of PAGE_SIZE.
When I build this to use memory allocated by kmalloc, the encryption succeeds, but when I build it to use the global array, buf, the encryption fails with the following error:
caam_jr 2142000.jr1: 40001016: DECO: desc idx 16: DMA Error
I'm running this on an iMX6UL with a 3.14.38 kernel. Why does global array test fail? Thank you.
//#define USE_KMALLOC
#define TVMEMSIZE 4
#define BUFFSIZE 128
static char *tvmem[TVMEMSIZE];
static u32 block_sizes[] = { 16, 0 };
static u8 speed_template_16[] = {16};
static char buf[BUFFSIZE*TVMEMSIZE];
static int __init testmodule_init(void)
{
int i;
#ifndef USE_KMALLOC
char* buffer = buf;
#else // USE_KMALLOC
char* buffer = (char*)kmalloc(BUFFSIZE*TVMEMSIZE, GFP_KERNEL);
#endif // USE_KMALLOC
for (i = 0; i < TVMEMSIZE; i++)
{
tvmem[i] = buffer + i*BUFFSIZE;
}
test_acipher_speed("ecb(aes)", ENCRYPT, 0, NULL, 0, speed_template_16);
#ifdef USE_KMALLOC
if (buffer)
{
kfree(buffer);
}
#endif // USE_KMALLOC
return 0;
}
解決済! 解決策の投稿を見る。
Hello,
Yes, it is needed to use the GFP_DMA flag of the kmalloc, which is used to specify that the allocator
must satisfy the request from ZONE_DMA. This flag is used by device drivers, which need DMA-able
memory for their devices.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I think I figured out the reason for DMA Error.
In linux kernel documentation https://www.kernel.org/doc/Documentation/DMA-API-HOWTO.txt, What memory is DMA'able? section it says
"If you acquired your memory via the page allocator (i.e. __get_free_page*()) or the generic memory allocators (i.e. kmalloc() or kmem_cache_alloc()) then you may DMA to/from that memory using the addresses returned from those routines.
:
This rule also means that you may use neither kernel image addresses (items in data/text/bss segments), nor module image addresses, nor stack addresses for DMA"
Hello,
Yes, it is needed to use the GFP_DMA flag of the kmalloc, which is used to specify that the allocator
must satisfy the request from ZONE_DMA. This flag is used by device drivers, which need DMA-able
memory for their devices.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri,
Now I'm trying to use the secure-memory as the source and destination with CAAM async-block ciphers through Linux crypto-API. I obtain the source and destination slots from secure-memory using sm_keystore_slot_alloc as shown below in the code segment. Error checking has been omitted for brevity here, but I do check for errors in the real code.
The crypto operation completes successfully, but when I check the dst location, it's contents remain the same, as if no crypto operation occurred. Why is this happening?
Thank you!
:
u8 __iomem *src, *dst;
struct caam_drv_private_sm *kspriv = dev_get_drvdata(ksdev);
sm_establish_keystore(ksdev, 1);
sm_keystore_slot_alloc(ksdev, 1, slotsize, &keyslot1);
src = kspriv->slot_get_address(ksdev, 1, keyslot1);
sm_keystore_slot_alloc(ksdev, 1, slotsize, &keyslot2);
dst = kspriv->slot_get_address(ksdev, 1, keyslot2);
// use src and dst with CAAM
:
Hello,
perhaps we have the same cache coherence issue ?
Are there CAAM errors ?
Regards,
Yuri.
Hi Yuri,
CAAM doesn't report any error. It says the operation is successful.
Can you please explain how cache coherency could come in here?
Thanks
Hello,
As for coherency : all buffers should not be cached.
Regards,
Yuri.