CAAM - SHA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAAM - SHA

2,021 次查看
jessicapujol
Contributor I

Hello,

I am trying to use the CAAM on iMX6.

Using the supplied SDK, I managed to implement the component and use AES ECB 128 successfully.
Now I have to use the SHA-1 but when I run the job ring, the CAAM hangs on.
The descriptor is as follows:

0xB0800006

0x8441000D

0x24140010

@Pointer to plain text buffer

0x60300010

@pointer to ciphered text buffer

Do you have any idea of the error in my descriptor ?

Thanks

Jessica  

标记 (1)
0 项奖励
回复
2 回复数

1,781 次查看
jessicapujol
Contributor I

Hello Yuri,

Thanks for the link but the guy does not explain which bits were wrong so I do not know if we have the same problem and how he solved it.

Jessica

0 项奖励
回复

1,781 次查看
Yuri
NXP Employee
NXP Employee

Hello

  Please look at https://community.nxp.com/message/654699 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复