Hello,
I'm trying to use ecspi2 on the i.MX8M Mini EVK using spidev.
I've followed the hint of the following topic to set spidev :
https://community.nxp.com/thread/502230
My main question is the following one :
Why the chip select toggle between each byte sent whereas I send 255 byte each time?
I use the following simple code :
static void transfer(int fd, uint8_t const *tx, uint8_t const *rx, size_t len)
{
int ret;
struct spi_ioc_transfer tr = {
.tx_buf = (unsigned long)tx,
.rx_buf = (unsigned long)rx,
.len = len,
.delay_usecs = delay,
.speed_hz = speed,
.bits_per_word = bits,
};ret = ioctl(fd, SPI_IOC_MESSAGE(1), &tr);
if (ret < 1)
pabort("can't send spi message");
}...
uint8_t default_tx[255] ;
uint8_t default_rx[ARRAY_SIZE(default_tx)] = { 0, };for (i = 0; i < SIZESPI; i++)
default_tx[i] = i;
transfer(fd, default_tx, default_rx, sizeof(default_tx));
Using a scope, I see that the chip select timing is pretty strict but its value change 255 times.
Best regards,
Frederic
Hi Frederic
one can check parameter BURST_LENGTH in ECSPIx_CONREG register
described in sect.10.1.5.3 Control Register (ECSPIx_CONREG)
i.MX 8M Mini Applications Processor Reference Manual
Also one can find ecspi examples with burst=8 in SDK_EVK-MIMX8M Mini
available on Welcome | MCUXpresso SDK Builder
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
ecspi registers can be found in Chapter 2 Memory Map Reference Manual
memtool can be used for reading registers
memtool\test - imx-test - i.MX Driver Test Application Software
Best regards
igor