Buildroot on mx6slevk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Buildroot on mx6slevk

1,350件の閲覧回数
arthurlambert
Contributor I

Hi,

I would like to use Buildroot to generate a linux for imx6 sololitevk.

I found an existing configuration done for this board in the master

branch of Buildroot.

To generate my image :

make freescale_imx6sololiteevk_defconfig

make all

Then I used this script in

board/freescale/imx6sabresd/create-boot-sd.sh to generate an sd card

by typing :

sudo ./create-boot-sd.sh /dev/mmcblk0

When I tried to run my sdcard on the board current result is :

reading uImage

5258568 bytes read in 267 ms (18.8 MiB/s)

Booting from mmc ...

reading imx6sl-evk.dtb

33925 bytes read in 18 ms (1.8 MiB/s)

## Booting kernel from Legacy Image at 80800000 ...

   Image Name:   Linux-3.10.17

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    5258504 Bytes = 5 MiB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 83000000

   Booting using the fdt blob at 0x83000000

   Loading Kernel Image ... data abort

    MAYBE you should read doc/README.arm-unaligned-accesses

pc : [<bff939d8>]          lr : [<bff70ee8>]

sp : bfc6b9d0  ip : 00000000     fp : 00000000

r10: 80d03d48  r9 : 00000000     r8 : bfc6bf38

r7 : 80800000  r6 : 00000000     r5 : bfc6ba14  r4 : 10008000

r3 : 00000000  r2 : 00503d08     r1 : 80800040  r0 : 10008000

Flags: Nzcv  IRQs off  FIQs off  Mode SVC_32

Resetting CPU ...

resetting ...

Is it normal ? Do I wrong somewhere in my process ?

Do I must add a patch on uboot-imx to fix that ?

I see some stuff like this for example :

https://gitorious.org/rowboat/u-boot/commit/7894b625259b89cd117685a0855a2c84b11a38f5

Thanks & Regards,

Arthur.

タグ(3)
0 件の賞賛
返信
0 返答(返信)