Building u-boot for imx8mm_evk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Building u-boot for imx8mm_evk

2,337件の閲覧回数
mahmed
Contributor I

Hi,

I'm trying to build and bring up U-boot for imx8mm_evk board. It looks like imx8 requires bunch of files to build the bootloader. The file that will eventually be put onto SD card is called 'imx-boot' genereated by imx_mkimage tool in combination of following four files: SPL, U-boot, ARM Trusted Firmware, DDR firmware.
My question is where do I get DDR firmware from. One of the README files say following but I can't access the repository:

1. DDR PHY firmware images (Mandatory, used for all targets)
Files: lpddr4_pmu_train_imem.bin and lpddr4_pmu_train_dmem.bin
Git: ssh://[email protected]/imx/linux-firmware-imx.git
Directory: firmware/ddr/synopsys

Any help is appreciated.

タグ(5)
0 件の賞賛
返信
1 返信

1,736件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello

Unfortunately, we still do not have support for the i.MX8MM since the product is still in preproduction and we do not have a way to test the problem. I apologize for the inconveniences.

Best regards,

Diego.

0 件の賞賛
返信