I have downloaded t he 10.0.0_2.3.0 Android build for the imx8mm Mini, and went through all the steps to setup the environment and project tree. I was able to build the bootloader, kernel, and rest of system the first time through.
I Had made a couple of changes to swap out for a different PMIC (PCA9450), and tried to recompile the bootloader and now I get this error messages (attached).
Since I first thought maybe something I had changed, I reverted my changes and tried to build again same thing.
So after trying many other things I came to desperation and completely removed the android_build folder and re-synced to the repo. Now on this fresh install, I get the same attached errros.
已解决! 转到解答。
I know this is an error with one of the many make files, but I got this message after removing the android_build folder and the /bin/repo and re-syncing to the project. Can someone please check the build tree to see if there an issue with it.
Thanks