Hi,
I have i.MX6UL SBC development board
I have downloaded source code using:
$ repo init -u https://github.com/Freescale/fsl-community-bsp-platform -b dora
I didn't find board name under :
source/meta-fsl-arm/conf/machine
with imx6ul...
only contains imx6dlsabresd.conf
Did I downloaded right copy of source code?
If yes, how to build images for imax6ul
and if not, which version of source code shall be used for imax6ul
Thank you
David Zhou
已解决! 转到解答。
Hi David,
the list below shows the machine names available, as you can see the machine available for i.MX6UL is imx6ulevk that provides configuration for i.MX6 Ultra Lite Evaluation Kit
This information can be fount in the in Freescale Yocto Project User's Guide
As I can see you are using a community BSP.
Please note that there are BSPs for i.MX processors developed by NXP and there are also BSPs created by a community external to NXP such as the one you are referring to.
You can find the NXP BSPs releases on git.freescale.com > fsl-arm-yocto-bsp.git
On the other hand the BSPs releases developed by the external community can be found here: https://github.com/Freescale/
NXP provides support of the BSPs developed by NXP, but unfortunately the releases of the external community are out of our scope.
If you need further support on any of the community's releases you may subscribe the FSL Community BSP mailing list at freescale.github.io to talk directly with the developers and other users.
Best regards,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi David,
the list below shows the machine names available, as you can see the machine available for i.MX6UL is imx6ulevk that provides configuration for i.MX6 Ultra Lite Evaluation Kit
This information can be fount in the in Freescale Yocto Project User's Guide
As I can see you are using a community BSP.
Please note that there are BSPs for i.MX processors developed by NXP and there are also BSPs created by a community external to NXP such as the one you are referring to.
You can find the NXP BSPs releases on git.freescale.com > fsl-arm-yocto-bsp.git
On the other hand the BSPs releases developed by the external community can be found here: https://github.com/Freescale/
NXP provides support of the BSPs developed by NXP, but unfortunately the releases of the external community are out of our scope.
If you need further support on any of the community's releases you may subscribe the FSL Community BSP mailing list at freescale.github.io to talk directly with the developers and other users.
Best regards,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------