Hi expert,
I am building AGL demo platform for imx8 following this guide: meta-nxp-agl - i.MX Yocto Project AGL Demo Layer ,
but I got some error while building. The log build as below:
ERROR: agl-service-data-persistence-1.0+gitAUTOINC+7147b65d07-r0 do_configure: Function failed: do_configure (log file is located at /data/workspace/linux-auto/imx8qxp-build/tmp/work/aarch64-poky-linux/agl-service-data-persistence/1.0+gitAUTOINC+7147b65d07-r0/temp/log.do_configure.15534)
ERROR: Logfile of failure stored in: /data/workspace/linux-auto/imx8qxp-build/tmp/work/aarch64-poky-linux/agl-service-data-persistence/1.0+gitAUTOINC+7147b65d07-r0/temp/log.do_configure.15534
Log data follows:
| DEBUG: Executing shell function do_configure
| -- The C compiler identification is GNU 7.3.0
| -- The CXX compiler identification is GNU 7.3.0
| -- Check for working C compiler: /data/workspace/linux-auto/imx8qxp-build/tmp/work/aarch64-poky-linux/agl-service-data-persistence/1.0+gitAUTOINC+7147b65d07-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux/aarch64-poky-linux-gcc
| -- Check for working C compiler: /data/workspace/linux-auto/imx8qxp-build/tmp/work/aarch64-poky-linux/agl-service-data-persistence/1.0+gitAUTOINC+7147b65d07-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux/aarch64-poky-linux-gcc -- works
| -- Detecting C compiler ABI info
| -- Detecting C compiler ABI info - done
| -- Detecting C compile features
| -- Detecting C compile features - done
| -- Check for working CXX compiler: /data/workspace/linux-auto/imx8qxp-build/tmp/work/aarch64-poky-linux/agl-service-data-persistence/1.0+gitAUTOINC+7147b65d07-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux/aarch64-poky-linux-g++
| -- Check for working CXX compiler: /data/workspace/linux-auto/imx8qxp-build/tmp/work/aarch64-poky-linux/agl-service-data-persistence/1.0+gitAUTOINC+7147b65d07-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux/aarch64-poky-linux-g++ -- works
| -- Detecting CXX compiler ABI info
| -- Detecting CXX compiler ABI info - done
| -- Detecting CXX compile features
| -- Detecting CXX compile features - done
| CMake Error at conf.d/cmake/config.cmake:204 (include):
| include could not find load file:
|
| CMakeAfbTemplates
| Call Stack (most recent call first):
| CMakeLists.txt:21 (include)
Even built for imx6qpsabreauto, I still got the same error.
Can anyone help me to fix it?
Many thanks!
Tung.
when you build for imx6qp auto, did you clean after building for imx8? I suggest that you need to clean then build for imx6qp auto
Hi Joan Xie, I've already cleaned after building for imx8 and still got the same build error.
I built this image for you, and I got error either, but my error isn't the same as yours, and my network has some issue, I'm not sure if my error is affected by network, I checked other customers built 4.1.15 succesfully, maybe you can try to built 4.1.15, this one is tested by development team
https://community.nxp.com/message/957677?commentID=957677#comment-957677
The repo init fails saying CES demo apps not available, Please share the exact correct and proven steps exclusive for AGL.
Thanks and Regards
Mani