Bringing up MCIMX6DLAICPU2 board.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bringing up MCIMX6DLAICPU2 board.

438件の閲覧回数
ramanareddy
Contributor I

Hi,

I have a board with MCIMX6DLAICPU2 processor. I want to bring this up. I tried loading the u-boot image compiled for imx6dlsabreauto which did not work.

 Where do I get the u-boot configuration for this board and also where to get dtb files for this board?

Thanks in advance

ラベル(3)
タグ(2)
0 件の賞賛
1 返信

373件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ramana Reddy,

You may find the demo images for the latest Linux release (L4.1.15_2.0.0) on the link below (please note you may need to login to download this file), which includes the i.MX6DL SABRE AI.

https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_MX6QDLSOLO&appType=license&Parent_nodeId=1...

You may also be interested on the L4.1.15 BSP Documentation, which includes instructions on how to build an image for the board (link below).

https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS

I’m curious on where did you found the image that is not currently working. If it’s one of the built images it’s possible that the u-boot wasn’t the right one for your board and the boot source you are using.

I hope this helps!

Regards,

0 件の賞賛