Hello,
I am working with imx8mp-evk with Yocto Linux.
I pull the Yocto linux from “repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.71-2.2.0.xml”
I compiled core-image-minimal, and I tested with imx8mp-evk.
With core-image-minimal I am not able to access wifi/BT.
Can you suggest how I can bring up WIFI/BT with imx8mp-evk with Yocto Linux minimal OS.
Thanks, in Advanced.
Solved! Go to Solution.
Hi @rathom3
To enable Wifi/BT for minimal OS, you need to manually compile its drivers and load it, also including firmware.
You can get driver from: http://source.codeaurora.org/external/imx/mwifiex.git
git checkout to newest tag.
firmware: https://github.com/NXP/imx-firmware/tree/lf-5.10.72_2.2.0/nxp
If you meet issue about compiling and need further support, please raise a new case with documenting compiling Wifi/BT for minimal yocto image. then the case will be got support from our Wifi/BT team's support.
Best regards
Harvey
Hi @rathom3
To enable Wifi/BT for minimal OS, you need to manually compile its drivers and load it, also including firmware.
You can get driver from: http://source.codeaurora.org/external/imx/mwifiex.git
git checkout to newest tag.
firmware: https://github.com/NXP/imx-firmware/tree/lf-5.10.72_2.2.0/nxp
If you meet issue about compiling and need further support, please raise a new case with documenting compiling Wifi/BT for minimal yocto image. then the case will be got support from our Wifi/BT team's support.
Best regards
Harvey
Hello @Harvey021
I am able to compile the driver moal.ko and mlan.ko with the help of "UM11675
How to Download and Build NXP Wi-Fi Drivers" Document and I downloaded the firmware according to my kernel version.
but I am unable to install modules to my core-image-minimal
Can you help me out in that area to install my modules to minimal image.
Thanks
Hi
You can refer to the document (https://www.nxp.com/webapp/Download?colCode=UM11483) to bring up respective of Wifi/BT module.
The document might be helpful for you: How to Integrate 88W8997 to iMX8MM-EVK & L5.4.24_2... - NXP Community
Best regards
Harvey
Hello @Harvey021 ,
i followed the steps and when i am trying to load the modules with command "modprobe moal mod_para=nxp/wifi_mod_para.conf "
Then i am getting below error
"[ 1705.120012] mlan: unknown parameter 'mod_para' ignored"
looks like module is loaded but ignoring the mod_para
Thanks,
Hi
Not sure what error it is. Can you check if there is directory /lib/firmware/nxp/ and then any difference comparing with normal wifi_mod_para.conf.
Best regards
Harvey