I am using IMX8ULP-EVk9 and In that I want to bring up bluetooth module(BGM220P)
BGM220P bilongs to silicon labs and to bring up that standalone we need to flash bt-ncp firmware from siliconlabs studio and test pairing of bluetooth, that process I completed I loaded bt-ncp firmware and paired device with my mobile bluetooth.
Now I want to start communication of BGM220P with IMX8ULP-EVK9's A core, and for that I am planning to use lpuart7.
To start communication which steps I need to follow so I can use BGM220P module from A core of IMX8ULP-EVK9 over lpuart7?
I also checked that lpuart7 is already enabled in dts file.