following the combination of the yocto project documentation and the manifest located at the github (https://github.com/nxp-imx/imx-manifest) for the yocto project am able to build the imx-image-multimedia image but when i go to build the imx-image-full i get this error:
WARNING: softhsm-2.6.1-r0 do_fetch: Failed to fetch URL https://dist.opendnssec.org/source/softhsm-2.6.1.tar.gz, attempting MIRRORS if available
WARNING: python3-matplotlib-3.6.3-r0 do_unpack: Failed to find a git repository in WORKDIR: /home/UTI/michael.jacobson/imx-yocto-bsp/bld-xwayland/tmp/work/armv8a-poky-linux/python3-matplotlib/3.6.3-r0
WARNING: qtbase-6.5.0-r0 do_package: KeyError in ./package/usr/lib/qtbase
ERROR: qtbase-6.5.0-r0 do_package: Error executing a python function in exec_func_python() autogenerated:
The stack trace of python calls that resulted in this exception/failure was:
File: 'exec_func_python() autogenerated', lineno: 2, function: <module>
0001:
*** 0002:sstate_report_unihash(d)
0003:
File: '/home/UTI/michael.jacobson/imx-yocto-bsp/sources/poky/meta/classes-global/sstate.bbclass', lineno: 903, function: sstate_report_unihash
0899: report_unihash = getattr(bb.parse.siggen, 'report_unihash', None)
0900:
0901: if report_unihash:
0902: ss = sstate_state_fromvars(d)
*** 0903: report_unihash(os.getcwd(), ss['task'], d)
0904:}
0905:
0906:#
0907:# Shell function to decompress and prepare a package for installation
File: '/home/UTI/michael.jacobson/imx-yocto-bsp/sources/poky/bitbake/lib/bb/siggen.py', lineno: 649, function: report_unihash
0645:
0646: if "." in self.method:
0647: (module, method) = self.method.rsplit('.', 1)
0648: locs['method'] = getattr(importlib.import_module(module), method)
*** 0649: outhash = bb.utils.better_eval('method(path, sigfile, task, d)', locs)
0650: else:
0651: outhash = bb.utils.better_eval(self.method + '(path, sigfile, task, d)', locs)
0652:
0653: try:
File: '/home/UTI/michael.jacobson/imx-yocto-bsp/sources/poky/bitbake/lib/bb/utils.py', lineno: 434, function: better_eval
0430: if extraglobals:
0431: ctx = copy.copy(ctx)
0432: for g in extraglobals:
0433: ctx[g] = extraglobals[g]
*** 0434: return eval(source, ctx, locals)
0435:
0436:@contextmanager
0437:def fileslocked(files, *args, **kwargs):
0438: """Context manager for locking and unlocking file locks."""
File: '<string>', lineno: 1, function: <module>
File "<string>", line 1, in <module>
File: '/home/UTI/michael.jacobson/imx-yocto-bsp/sources/poky/meta/lib/oe/sstatesig.py', lineno: 650, function: OEOuthashBasic
0646: update_hash("\n")
0647:
0648: # Process this directory and all its child files
0649: if include_root or root != ".":
*** 0650: process(root)
0651: for f in files:
0652: if f == 'fixmepath':
0653: continue
0654: process(os.path.join(root, f))
File: '/home/UTI/michael.jacobson/imx-yocto-bsp/sources/poky/meta/lib/oe/sstatesig.py', lineno: 593, function: process
0589: except KeyError as e:
0590: bb.warn("KeyError in %s" % path)
0591: msg = ("KeyError: %s\nPath %s is owned by uid %d, gid %d, which doesn't match "
0592: "any user/group on target. This may be due to host contamination." % (e, path, s.st_uid, s.st_gid))
*** 0593: raise Exception(msg).with_traceback(e.__traceback__)
0594:
0595: if include_timestamps:
0596: update_hash(" %10d" % s.st_mtime)
0597:
File: '/home/UTI/michael.jacobson/imx-yocto-bsp/sources/poky/meta/lib/oe/sstatesig.py', lineno: 587, function: process
0583: else:
0584: add_perm(stat.S_IXOTH, 'x')
0585:
0586: try:
*** 0587: update_hash(" %10s" % pwd.getpwuid(s.st_uid).pw_name)
0588: update_hash(" %10s" % grp.getgrgid(s.st_gid).gr_name)
0589: except KeyError as e:
0590: bb.warn("KeyError in %s" % path)
0591: msg = ("KeyError: %s\nPath %s is owned by uid %d, gid %d, which doesn't match "
Exception: Exception: KeyError: 'getpwuid(): uid not found: 113990'
Path ./package/usr/lib/qtbase is owned by uid 113990, gid 110513, which doesn't match any user/group on target. This may be due to host contamination.
ERROR: Logfile of failure stored in: /home/UTI/michael.jacobson/imx-yocto-bsp/bld-xwayland/tmp/work/armv8a-poky-linux/qtbase/6.5.0-r0/temp/log.do_package.602736
ERROR: Task (/home/UTI/michael.jacobson/imx-yocto-bsp/sources/meta-qt6/recipes-qt/qt6/qtbase_git.bb:do_package) failed with exit code '1'
it looks like it is expecting me to be userID 113990, which i am not, apparently
i'm not entirely sure what to do about it
解決済! 解決策の投稿を見る。
so our avnet rep told us that 6.1.36 was not available yet for the 93evk board and, really, we should build with kirkstone. so i blew away our whole directory and started over with kirkstone 5.15.71 and it did eventually build. thanks for your help
so our avnet rep told us that 6.1.36 was not available yet for the 93evk board and, really, we should build with kirkstone. so i blew away our whole directory and started over with kirkstone 5.15.71 and it did eventually build. thanks for your help
Thank you for contacting NXP Support.
I'm trying to replicate your issue on my side, especially I'm looking the reason to the error on fetch URL.
Regarding the errors about User ID, I found a reference discussing your same issue.
It seems that you can avoid the error using:
"It helped to add 'chown -R root.root ${D}${libdir}'. Thanks!"
Here is the link: yocto@lists.yoctoproject.org | Help and ideas wanted - error during do_package
Please try this solution and tell me if it works!
Have a great day!
the fetch error is likely our internet filter, don't waste your time on that
where do i add that? in qtbase_git.bb in the do_install? i'm not an expert at this. can i just sudo chown the source dir?
Yes, based on your error you will need to add the command "chown -R root. Root ${D}${libdir}" in section "do_install" in the recipe qtbase_git.bb, located on the path: ../sources/meta-qt6/recipes-qt/qt6.
Please try and tell me if it works.
Have a great day!