I'm following the "Android Quick Start Guide, Rev kk4.4.2_1.0.0-ga, 07/2014". I've downloaded the board image (Download target - SD) successfully and would like to boot via HDMI. In the iMX6SL section, the guide only provides the commands to boot via the LCD.
5.4 Booting with single display: LCD display
UBoot > setenv bootcmd booti mmc1
UBoot > setenv bootargs console=ttymxc0,115200 init=/init
androidboot.console=ttymxc0 video=mxc_elcdif_fb:bpp=32
androidboot.hardware=freescale csi
UBoot > saveenv
I've tried using the commands used in "4 Working with SABRE-AI Board" for booting via HDMI by modifying them a bit.
Does this build support booting from HDMI since those commands are missing in the iMX6SL section of the document? If not what the solution?
yes, if you use mx6slevk board, which can support hdmi output.
<i.MX 6SoloLite Evaluation Kit|Freescale>.
display board interface:
I tested this on my mx6slevk baord successfully, only change is that :
> set bootargs 'console=ttymxc0,115200 init=/init anddroidboot.console=ttymxc0 panel=hdmi'
>save
>run bootcmd