Booting issue in imx6 kontron board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting issue in imx6 kontron board

2,669 Views
joevince
Contributor II

Hai...

we are using third party board of kontron(smarc -samx6i) using imx6.we are trying to boot using the Yocto document attached here.

U-Boot 2015.04-00025-gaa1cf09 (Jul 21 2015 - 15:28:22)

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz
Board: Kontron SMARC-sAMX6
I2C:   ready
DRAM:  1 GiB
MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
SF: Detected W25Q16DW with page size 4 KiB, total 2 MiB
SF: Detected W25Q16DW with page size 4 KiB, total 2 MiB
Display: LCD_1024x768@LVDS (Resolution: 1024x768 [px], LVDS clk 72 [MHz])
In:    serial
Out:   serial
Err:   serial
Selected Boot source: Carrier SD Card
Net:   FEC [PRIME]
Hit any key to stop autoboot:  0
49272 bytes read in 104 ms (461.9 KiB/s)
4565488 bytes read in 264 ms (16.5 MiB/s)
## Booting kernel from Legacy Image at 10800000 ...
   Image Name:   Linux-3.10.17-rel1.0+g232293e
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    4565424 Bytes = 4.4 MiB
   Load Address: 10008000
   Entry Point:  10008000
   Verifying Checksum ... OK
Wrong Ramdisk Image Format
Ramdisk image is corrupt or invalid

could anyone help?

0 Kudos
Reply
4 Replies

1,826 Views
igorpadykov
NXP Employee
NXP Employee

Hi berlin

seems for Linux-3.10.17 uboot 2013.04 should be used.

What images are used in the case, are they customized for this board,

obtained from kontron bsps ? In general best way to ask support from

vendor of that board:

Contact Support - Kontron

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,826 Views
joevince
Contributor II

Thanks for your reply,

We use uimage as .bin file and zimage as .dtb file and are customized for kontron(smarc samx6i).

What could be the reason for the error ,

Wrong Ramdisk Image Format
Ramdisk image is corrupt or invalid

Best regards

0 Kudos
Reply

1,826 Views
simon_cai
Contributor III

Hi berlin vince

Maybe I can try and reproduce this situation & issue in my Kontron SMARC board,

Please send me the BSP Components or just the "smarc-samx6i-support-R01.00.diff" file,

Let me try to fix it.

BM

0 Kudos
Reply

1,826 Views
igorpadykov
NXP Employee
NXP Employee

seems more proper is to post it to meta-fsl-arm mailing list

or uboot mail list, as this is more general linux question:

https://lists.yoctoproject.org/listinfo/meta-freescale

~igor

0 Kudos
Reply