I've been working an image using U-Boot Falcon mode. With this technique is possible to boot i.MX6Q Sabre SD completely under one second. I recorded my results on: Booting i.MX6 Under One Second. If you want to get more details, please go to How to decrease boot time on iMX6 - i.MXDev Blog.
Very nice! As I'm also planning to use the Falcon mode soon, could you please share your U-Boot/Kernel?
Which init-system are you using? I guess it's just a plain shell, so no SysV/Busybox, SystemD or similar, right?
As init-system I'm using the default from Poky-tiny. You can get a full image here: Dropbox - falconmode_imx6sabresd.sdcard
For Kernel I'm using the stable version 4.7 and u-Boot I'm basing my work on master because I will upstream my patches.
Anything else you can contact me by e-mail.
This technique is already implemented on u-Boot. It's calls u-Boot Falcon Mode developed by Stefano Babic.
Of course there are a few more things involved, such as removing unused drivers from Kernel, also reducing the root file system to minimal size.
http://www.denx.de/wiki/pub/U-Boot/MiniSummitELCE2013/2013-ELCE-U-Boot-Falcon-Boot.pdf