Hello,
I'd like to boot my i.mx6 sabresd from network, using a tftp server. I've followed the Linux User's Guide.pdf, with some minor modifications.
setenv serverip IPADDR
setenv bootfile uImage
setenv fdt_file imx6q-sabresd.dtb
setenv ethaddr 00:04:9f:02:e2:33
saveenv
dhcp
mmc dev 1
mmc write ${loadaddr} 0x800 0x4000
tftpboot ${fdt_addr} ${fdt_file}
fdt addr ${fdt_addr}
setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk2p2 rootwait rw'
setenv bootcmd_mmc 'run bootargs_mmc;mmc dev 1;mmc read ${loadaddr} 0x800 0x4000;mmc read ${fdt_addr} 0x5000 0x800;bootm ${loadaddr} - ${fdt_addr}'
setenv bootcmd 'run bootcmd_mmc'
saveenv
But, when using boot (or bootd), I have the following :
switch to partitions #0, OK
mmc1 is current device
MMC read: dev # 1, block # 2048, count 16384 ... 16384 blocks read: OK
MMC read: dev # 1, block # 20480, count 2048 ... 2048 blocks read: OK
## Booting kernel from Legacy Image at 12000000 ...
Image Name: Linux kernel
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5578744 Bytes = 5.3 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... Bad Data CRC
ERROR: can't get kernel image!
There is an error with the checksum, but the zImage works fine for a classic booting.
To create the uImage, I've made : mkimage -A arm -O linux -T kernel -C none -a 0x80008000 -e 0x80008000 -n "Linux kernel" -d zImage uImage.
I've tried with zImage (without converting to uImage), but it doesn't work event with bootz.
You are booting from MMC.
Are you want to boot from NFS?
According to the User Guide,
4.7.5 Running the Linux Image From NFS
To boot from NFS, set the following environment variables at the U-Boot prompt:
U-Boot > setenv serverip 10.192.225.216
U-Boot > setenv image <your kernel zImage name on the TFTP server>
U-Boot > setenv fdt_file <your dtb image name on the TFTP server>
U-Boot > setenv rootfsinfo 'setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:/data/rootfs_home/rootfs_mx6,v3,tcp'
U-Boot > setenv bootcmd_net 'run rootfsinfo; dhcp ${image}; dhcp ${fdt_addr} ${fdt_file}; bootz ${loadaddr} - ${fdt_addr}'
U-Boot > setenv bootcmd 'run bootcmd_net'
NOTE
If the MAC address has not been burned into the fuses, you must set the MAC address to
use the network in U-Boot.
setenv ethaddr xx:xx:xx:xx:xx:xx
Booting with nfs isn't exactly what I'd like to do. My idea is to do as if I was using PXE : downloading kernel, booting on it, donwloading rootfs, and end of the boot (of course, I could download the rootfs in the same time than the kernel). I just want to download all the necessary, to use the card without network. Is it possible ?
By curiosity, I've tried to boot on nfs (I had already read the user's guide, but never tested). Here is what I do :
U-Boot >setenv serverip 192.168.1
U-Boot >setenv rootfsinfo 'setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:/images/core-image-x11-imx6qsabresd.ext3,v3,tcp'
U-Boot >setenv bootcmd_net 'run rootfsinfo; dhcp ${image}; tftpboot ${fdt_addr} ${fdt_file} ;fdt addr ${fdt_addr} ; bootz ${loadaddr} - ${fdt_addr}'
U-Boot >setenv bootcmd 'run bootcmd_net'
U-Boot >saveenv
But the booting stops at "starting kernel". If I do the same without NFS, it works (but I have a kernel panic later because it doesn't find the rootfs) :
U-Boot >setenv bootcmd_net 'run rootfsinfo; dhcp ${image}; tftpboot ${fdt_addr} ${fdt_file} ;fdt addr ${fdt_addr} ; bootz ${loadaddr} - ${fdt_addr}'
U-Boot >setenv bootcmd_net 'dhcp ${image}; tftpboot ${fdt_addr} ${fdt_file} ;fdt addr ${fdt_addr} ; bootz ${loadaddr} - ${fdt_addr}'
Any idea why ?