Booting from SD card but running on QSPI for IMX6ULL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Booting from SD card but running on QSPI for IMX6ULL

1,351 次查看
fabio_poiatti
Contributor III

Hi everyone,

my application starts from SD card flashed from custom kernel coming from 4.14.78-r0.

My intention would be keep the boot from SD card but use the application ruuning from QSPI.

Is it possible to do that easily?

thanks

Fabio

0 项奖励
回复
6 回复数

1,256 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Fabio

seems most easy way to run m4 core from qspi using examples from

SDK2.2_iMX6ULL_WIN

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,256 次查看
fabio_poiatti
Contributor III

Sorry Igor,

I didn't understand.

Where I have to look for? 

Absolutely I need to have the sd card for booting the board and also for the application ... but

I was thinking something like move the application on qspi to run ...

thanks

Fabio

0 项奖励
回复

1,256 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Fabio

I think one can use approach described in sect.5.2 Using Manufacturing Tool attached

Getting Started with MCUXpresso SDK for i.MX 6ULL Derivatives.pdf

check for "b. QSPI XIP image".

Best regards
igor

0 项奖励
回复

1,256 次查看
fabio_poiatti
Contributor III

Sorry Igor

I need also only a simple test to check the QSPI for hardware validation ...

Is it possible via unit_test?

Thanks

FAbio

0 项奖励
回复

1,256 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Fabio

there are some qspi tests in

SDK2.2_iMX6ULL_LINUX

Best regards
igor

0 项奖励
回复

1,256 次查看
fabio_poiatti
Contributor III

Hi 

there is the posibility to have a similar tool for linux system?

thanks

Fabio

0 项奖励
回复