Hi everyone,
my application starts from SD card flashed from custom kernel coming from 4.14.78-r0.
My intention would be keep the boot from SD card but use the application ruuning from QSPI.
Is it possible to do that easily?
thanks
Fabio
Hi Fabio
seems most easy way to run m4 core from qspi using examples from
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Sorry Igor,
I didn't understand.
Where I have to look for?
Absolutely I need to have the sd card for booting the board and also for the application ... but
I was thinking something like move the application on qspi to run ...
thanks
Fabio
Sorry Igor
I need also only a simple test to check the QSPI for hardware validation ...
Is it possible via unit_test?
Thanks
FAbio
Hi
there is the posibility to have a similar tool for linux system?
thanks
Fabio