Booting Android on i.MX53 QSB from SD: not mounting /system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting Android on i.MX53 QSB from SD: not mounting /system

ソリューションへジャンプ
1,348件の閲覧回数
alexandremedeir
Contributor I

Hello, I'm trying to boot Android on my i.mx53 qsb but I'm having some problems, aparently the /system partition is not mounting, so the kernel boots but there's no program to run, the funny thing is that I get a tux picture on my vga monitor...

 

I'm using Adeneo's prebuilt Freescale-iMX53-QSB-Android 2.3-Version 4.3 image, I tried following the i.MX Android R10.3.2 User Guide to boot from SD with the prebuilt image, but encountered the same problems, the main difference is that on Adeneo's image, the adb is launched, but my computer doesn't finds any device with the adb and I only get the tux picture with Adeneo's image.

 

When I connect the usb cable on my computer I see this message on the serial output:

 

usb wakeup is here

otg udc vbus rising wakeup

android_usb gadget: high speed config #1: android


I'm attaching the serial output from boot, I think it might help.

Thanks

Original Attachment has been moved to: imx53-android-log-adeneo_prebuilt.txt.zip

ラベル(2)
1 解決策
713件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

How did you partition your sdcard?

I saw it on your log:

mmc0: new high speed SDHC card at address 1234

mmcblk0: mmc0:1234 SA04G 3.67 GiB

mmcblk0: unknown partition table

Does your sdcard have any partition table?

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
714件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

How did you partition your sdcard?

I saw it on your log:

mmc0: new high speed SDHC card at address 1234

mmcblk0: mmc0:1234 SA04G 3.67 GiB

mmcblk0: unknown partition table

Does your sdcard have any partition table?

0 件の賞賛
713件の閲覧回数
alexandremedeir
Contributor I

Thanks, I didn't notice that the script deleted the partition table, I fixed and now it's working

713件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

Great!

0 件の賞賛