Hello all.
I am working to build a custom bootloader by using SDK. I have achieved to boot the custom board with only using the "u-boot.imx" inside the sdcard. However, when I try to write the "u-boot.imx" on a partitioned sdcard that includes the image that I built previously, the system uses the bootloader which is included the image itself, not the one that I have created using the SDK.
The procedure that I am following:
1.Writing the image on the sdcard using the "$ sudo dd if=<.sdcard image> of=/dev/sdb bs=1M" command.
2.Writing the "u-boot.imx" file on the sdcard using the "$ sudo dd if=u-boot.imx of=/dev/sdb1 bs=1M seek=2 conv=fsync"
command.
(Additional question: The board does not boot without adding the "seek" part of the command. What is the reason of this? I will be more than happy, if you answer it.)
(I try to write the "u-boot.imx" on the first partition of the sdcard to avoid deleting the second partition.)
3.Try to boot it using the board.
4.Board uses the original u-boot (that is included inside the image itself) not the one that I have created using the SDK. I want to boot it with the SDK one.
(The date of compilation of the u-boot is Oct 03 2017 when I boot the device. I created the SDK one on Oct 09 2017. That is how I am telling it is using the other one. I do not know this is the correct way to tell it.)
I tried numerous solutions to solve this issue. However, none of them worked.
Many thanks.
已解决! 转到解答。
Hi Giray,
Please try the following command:
$ sudo dd if=u-boot.imx of=/dev/sdX bs=1K seek=1; sync
Remember to replace sdX with the correct partition mounted in your PC (possible sdb).
Thanks!
Vanessa
Hi Giray
also may be useful to check Linux Guide for programming images included in
sdcard image includes already uboot, so writing the "u-boot.imx" file on step 2
overwrites original image uboot.
Best regards
igor
Hi Giray,
Please try the following command:
$ sudo dd if=u-boot.imx of=/dev/sdX bs=1K seek=1; sync
Remember to replace sdX with the correct partition mounted in your PC (possible sdb).
Thanks!
Vanessa