Boot_cfg fuse issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Boot_cfg fuse issue

736 次查看
jimhuang2
Contributor III

Hi all,

With the rt1050 evkb, I need to check something about the Boot CFG[0:11], When Boot CFG[0:11] set up, The FDCB of the Boot image is error value, Can used the "NXP Boot Utility" rebuild or erase flash (Boot Mode= 0'b01) ?

I think it can, but I need a definitive answer.

I would like to directed against sample code of burning boot cfg[0:11] fused to reference, because I'm not sure, Is the program I wrote correct.

Best Regard

Jim

标签 (1)
1 回复

646 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi JingHuan Huang,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Can I use the "NXP Boot Utility" rebuild or erase the flash (Boot Mode= 0'b01)?
-- Yes, the NXP Boot Utility is able to erase the flash and burn the fuse map.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------