Hello, All
I'm beginner about imx6 processor. Checking functions with the SABREAUTO RDK board.
I was getting started with i.MX_Yocto_Project_User's_Guide.pdf inside of imx-yocto-L4.14.98_2.0.0_ga.tar.gz.
It worked everything - built a sdcard image with yocto, write it to sdcard with mfgtool and boot with sdcard.
The SABREAUTO RDK board has not the MMC chip, only it has the sdcard slot.
Custom board is not ready, it has a eMMC chip.
Check to select the MMC mode of boot options with the sdcard, before the board comes out.
I think it could boot a MMC mode with sdcard, but it didn't shows any messages on the serial port.
SDcard Boot: BOOT_CFG1 = 0100_1000b, BOOT_CFG2 = 0011_0010b
MMC Boot: BOOT_CFG1 = 0110_1000b, BOOT_CFG2 = 0011_0010b
The options are almost the same, changed a MMC mode.
Please let me advice about it.
Thanks.
Hi, Bio
Sorry too late.
The SABREAUTO board connected uSDH3 port which it is a SD/MMC-card slot.
I would like to check the MMC boot mode with this port which it is inserted SD/MMC-card.
Wait for a custom board to come it out. It must check with an EMMC chip.
Is it right ?
Regards