Hi XU
please look on
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Just 3.00?
In my PC, it's value is 5184.00.
Is there some thing wrong here?
3Q
you can try kernel 3.0.35 which had correct value.
change happens since: commit 1119c84aa3053bd415ba731ada1ecef24c8f82a2
Author: Sebastian Andrzej Siewior <bigeasy@linutronix.de>
Date: Wed Jan 22 12:35:44 2014 +0100
ARM: imx: enable delaytimer on the imx timer
The imx can support timer-based delays, so implement this.
Skips past jiffy calibration.