Board bringup of the customized board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Board bringup of the customized board

377 Views
srinivasaporam
Contributor II

Hi,

We have got IMX6D customized board, which is based on the IMX6D reference designs. Our board and reference board differs in Operating voltages. Reference board is based on 3.3V where as our customized board is designed to operate at 1.8V.

Will this difference in operating voltages makes any difference in bringing up board in software side (BSP Customization). What are all the files that need to be modified.

Labels (4)
0 Kudos
1 Reply

296 Views
igorpadykov
NXP Employee
NXP Employee

Hi Srinivasa

for i.MX6DQ only uSDHC module has voltage selection in register

uSDHCx_VEND_SPEC (VSELECT - controls the voltage on pads for external card),

for other modules voltage level is defined by its power supply value given in

Table 100 i.MX6DQ Datasheet (rev.4, 7/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos